Agency Listings and Approvals for the Continuum products

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Agency Listings and Approvals for the Continuum products
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1285 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Agency Listings and Approvals for the Continuum products

Picard Product_Support
‎2018-09-10 07:03 AM

Last Updated: Crewman ContentModerator ‎2025-10-15 03:37 AM

Issue

Different Continuum products are approved to different approval standards and where are copies of these certificates held?

Product Line

Andover Continuum

Environment

  • All Hardware products:
  • Standards listings to UL, BTL C-Tick, CE

Cause

Copies of the approval certificate or clarification on the different standards are required.

Resolution

The Agency listings each controller is approved against are defined on the datasheet, for more information see How do I get the part numbers and datasheets for Continuum products?.

An example of the approvals for the bCX1 controllers are:

UL/CUL 916, UL 864 9th Edition, FCC CFR 47 Part 15, ICES-003, EN55022,

AS/NZS 3548, Class A, VCCI, EN61000-6-1, CE

 

All of the Regulatory Compliance documents including: UL, CUL, ISO,  European CE Certificates, Australia/ New Zealand  C-Tick Certificates and WSP Cert can be downloaded from The Exchange Download Center -  Regulatory Compliance

 

Confirmation of BACnet testing can be seen at the BTL website:

http://www.bacnetinternational.net/btl/

European Standards -

Continuum has been tested to the following as part of the 89/336/EEC Electromagnetic Compatibility Directive and over the years the standards have changed.

Emissions -Continuum is tested against EN55022-Class A This is the emission standard for Information Technology equipment and another emission standard is the EN50081-1 but this is a generic emission level and less stringent than the IT standard that Continuum complies with.


Immunity - These standards have changed over the years, older controllers were tested against the International IEC1000-4 and we state the specific levels our controllers are tested against, then when it was released in 2000 we used the EN50082-1 standard which replaced the IEC standard in Europe. But newer controllers have now been tested against the EN61000-6-2  standard that have since replaced the other immunity standards. 
 

There is also the EN60730-1 standard that Continuum is approved to, this defines the standard controls specifications it can perform.


These standards are required for us to apply the CE marking to our products.

Labels (1)
Labels:
  • Andover Continuum
Tags (1)
  • Find more articles tagged with:
  • 6512
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.