Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84599members
353865posts

Somachine HVAC 2.4.1 Error Support

Ask the Community

New users can ask questions related to our Communities, get tips and tricks on posting and commenting in forums, and solving challenges.

HOANGTHINH
Lieutenant JG
Lieutenant JG
0 Likes
1
2583

Somachine HVAC 2.4.1 Error Support

I have a project of Somachine HVAC, but it has problem :

 

--- Start compilation : Wednesday, May 15, 2019 8:06:22 PM ---
DDC-B4F: created CANopen Master cfg 0 (3 slaves, 34 variables)
Extension ModbusCustom not found while calling ModbusCustom.GetDeviceParameters
SCRIPT ERROR! Descr: 'length' is null or not an object, Err: 17, LineNum: 2572, Code: (null)
Can not invoke function GetEDSInfo in extension M172P_596p6: error 0x80020101 'Unknown error 0x80020101'
ERROR: (WriteEDS) Invalid CAN data
CFN correctly saved as F:\GIA_HUY_ENGINEER\Du_An\2019\CZ - Slovakia\PROGRAM\DDC-B4F\DDC-B4F.CFN
--- End compilation : Wednesday, May 15, 2019 8:06:23 PM ---
Extension ModbusCustom not found while calling ModbusCustom.RunModbusCustomEditor
Extension ModbusCustom not found while calling ModbusCustom.RunModbusCustomEditor

 

 

I'trying to reinstall software but efective. Who can help me ? Please .

Thanks very much

 

 

Attachments
1 Reply 1
razgadi_work_gm
Ensign
Ensign
0
2536

Re: Somachine HVAC 2.4.1 Error Support

https://www.schneider-electric.com/en/product-range-download/62420-modicon-m171-m172/

 

Good Morning
Try to work with this version is much more perfect than its predecessors.
If it does not work out check the settings well.
You will add one each time and compile.
Successfully