Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2024-01-2808:16 AM
HSBT ,High speed bus transfer system controller
Hello Dears
General topic for HSBT for MV 11 KV SWG , it is required to have high speed bus transfer system . i searched found SUE 4000 in ABB meanwhile no equivalent in SE products , so i was wondering if some one faced this solution or worked for it in similar projects or with OG product as lots of signals and complicated logic need to be implemented as the SWG feeding critical MV motors