Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2024-12-2304:00 AM
Error 1006 atv 320 drives
Hello,
Just looking for a bit of help with a new vfd. We had a shaker, and a 5hp vfd configured with ethernet communication for control. They removed the shaker and put a 7.5 hp motor for a pump in its place. I tried to load the shaker program in, change the vfd my device settings to match the new vfd but I'm not sure what else to change for the software to load tge program into the new vfd. I get an "Error 1006" message about the dtm not.matching the device topology. Looking for a way to correct this. I'm a novice user at best so any help would be greatly appreciated