New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
UTS10BI and backup source 1
APC UPS for Home and Office Forum
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-2910:21 PM. Last Modified: 2024-03-2003:03 AM
UTS10BI and backup source 1
The default for backup source 1 is generator. But, there are options to set the source type to either UPS or 'other' as well. However, the manual doesnt say anything about how the UTS will behave differently if the backup source 1 type is set to either of these alternatives. I could make some guesses about setting it to UPS but I like to know for sure. As for the purpose of 'other', I'm stumpped and the manual doesnt help either.
If I connect a large 240v UPS instead of a generator to backup source 1, would there by any reason to still use a UPS as backup source 2? If both backup sources are set to UPS and two different UPS are used for each, which would power a circuit set to 'uninterruptable'? My hope is that when source 1 is a UPS, uninterruptable circuits would be powered by source 1 and source 2 would no longer be needed at all. Can anyone confirm this?