Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84590members
353857posts

Question about the J10

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
blackjackmark_apc
Crewman
Crewman
0 Likes
1
103

Question about the J10

This was originally posted on APC forums on 3/31/2013


Sorry if this is in the wrong forum, I could not seem to find one for the A/V product. But I recently purchased the J10 and am wanting to use the DC trigger feature. However, it seems that when the DC trigger is used, that it controls two sets of two outlets each. Each of those sets of two can have their delay customized, but what I would like to do would be to have the DC trigger only control one of the two pairs. Is there a way to do that? I really do not want 4 of the 12 outlets to completely shut down when the triggering device shuts down.

Tags (1)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
104

Re: Question about the J10

This reply was originally posted by Secret on APC forums on 4/1/2013


Unfortunately, their is not further customization of these receptacles. They are all controlled by the same DC Function simultaneously.  

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
105

Re: Question about the J10

This reply was originally posted by Secret on APC forums on 4/1/2013


Unfortunately, their is not further customization of these receptacles. They are all controlled by the same DC Function simultaneously.