Posted: 2023-05-11 01:44 PM
Question about battery connector for Bx2200mi-ar.
Hello, today my UPS Bx2200mi-ar arrived, and I had two questions when I wanted to install it.
1) Is it normal that there was a spark when I installed the battery connector for the first time, without ever having plugged the equipment into an electrical outlet before?
2) How far does the same connector have to go? I placed it and it seems that it is a little outside, but with a little force it doesn't go in anymore, and I don't want to force it unnecessarily (I attach a photo).
Thank you so much.
- Labels:
-
Home & Office - UPS & Software
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
Posted: 2023-05-15 08:24 AM
It is normal for a spark to be seen.
As for the connector, push it in until it makes contact but do not force it. The UPS will report if the battery is not connected.
Link copied. Please paste this link to share this article on your social media post.