Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Search in
Posted: 2021-06-28 10:58 PM . Last Modified: 2024-03-22 04:30 AM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-28 10:58 PM . Last Modified: 2024-03-22 04:30 AM
To Whom It May Concern,
I am in a bit of a situation here and I hope to get some good news haha. My desk at work has a notebook PC, a small lamp and a set of small speakers. However, the desk is positioned out of reach for my UPS ES 350. I am not able to move my desk and I was hoping someone could tell me which type of extension cable I could use with my ES 350.
I tried a long orange cable that is pretty heavy duty, but the red light (faulty building wiring) came on. Is it safe to assume that any cable I use which does not activate that red warning light is safe for use with the ES 350?
Once again. Is there a particular type fo extension cord I can use with the ES 350?
If the red warning lite does not come on, does this mean I have purchased a sufficient cable?
Thank you very much.
Best,
Jesse
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-28 10:59 PM . Last Modified: 2024-03-22 04:30 AM
Per National Electrical code, you are not supposed to use an extension cable.
The APC product must be plugged into properly wired and grounded outlets; no extension cords, adapters, other ground wires, or electrical connections may be used... as stated in National Electric Code (NEC) NFPA 70A, extension cords are considered temporary devices and should not be used for prolonged periods.
It may be possible to use an extension cable which are underrated for the power being pulled. This might lead to overheating of the wire and in worst case scenarios, melting of the wire. Extension cords may also become pinched or severed during normal or prolonged use, exposing others to raw power and a potential for electrocution. Customers might perceive such problems as a result of using the surge protector/UPS. It also might lead to damages to infrastructure, which may lead to EPP claims and disputes over responsibility.
Futhermore, a site/building wiring fault light indicates one or more of the following:
•Missing or loose ground wire
•Reversed polarity
•Overloaded neutral wire
You can check out those issues and see if you can figure out what it is.
So even though APC does not recommend the extension cables, if you find a suitable extension cord with the proper gauge wire, I supposed you could use but I still strongly recommend against it due to the above notes.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-28 10:59 PM . Last Modified: 2024-03-22 04:30 AM
Per National Electrical code, you are not supposed to use an extension cable.
The APC product must be plugged into properly wired and grounded outlets; no extension cords, adapters, other ground wires, or electrical connections may be used... as stated in National Electric Code (NEC) NFPA 70A, extension cords are considered temporary devices and should not be used for prolonged periods.
It may be possible to use an extension cable which are underrated for the power being pulled. This might lead to overheating of the wire and in worst case scenarios, melting of the wire. Extension cords may also become pinched or severed during normal or prolonged use, exposing others to raw power and a potential for electrocution. Customers might perceive such problems as a result of using the surge protector/UPS. It also might lead to damages to infrastructure, which may lead to EPP claims and disputes over responsibility.
Futhermore, a site/building wiring fault light indicates one or more of the following:
•Missing or loose ground wire
•Reversed polarity
•Overloaded neutral wire
You can check out those issues and see if you can figure out what it is.
So even though APC does not recommend the extension cables, if you find a suitable extension cord with the proper gauge wire, I supposed you could use but I still strongly recommend against it due to the above notes.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.