Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84660members
354047posts

BE600M1 with Business PowerChute

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
KHappe_apc
Cadet
0 Likes
1
119

BE600M1 with Business PowerChute

This was originally posted on APC forums on 5/11/2020


I have a media server at home and it is running Windows Server 2016.

I bought a a BE660M1 to help it weather power outages.

I can't install the personal version of PowerChute on the server, because it is a server.

So I installed the Business Version of PowerChute.  
The settings on the PowerChute Agent site, just dont make sense.

It says the battery is at 10% charge and has a voltage of 11.9 V

I installed PowerChute personal version on my pc and tried it from there.  It gave much better details that server agent.

Said it was fully charged etc.

So does the BE600M1 work with the Business version of PowerChute?
I dont really care if the details on the agent site aren't correct. I will be happy as long as it powers the server down gracefully when power fails.

 


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
119

Re: BE600M1 with Business PowerChute

This reply was originally posted by Bill on APC forums on 5/12/2020


Hi,

PowerChute Business Edition is not compatible with the BE600M1. Your options are, configure native power option is the control panel. See Schneider Electric FAQ FA159653. The other option is to install APCUPSD

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
120

Re: BE600M1 with Business PowerChute

This reply was originally posted by Bill on APC forums on 5/12/2020


Hi,

PowerChute Business Edition is not compatible with the BE600M1. Your options are, configure native power option is the control panel. See Schneider Electric FAQ FA159653. The other option is to install APCUPSD