Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

APC transfer switch UTS10BI circuit 9 & 10 for 240V

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • APC transfer switch UTS10BI circuit 9 & 10 for 240V
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
BillP Leader
2151
Teken
Teken
152
Techie_apc
Techie_apc
83
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
Back to APC UPS for Home and Office Forum
Start a Topic
PerOla
PerOla
Explorer

Posted: ‎2023-09-22 06:48 AM

0 Likes
0
858
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
Posted: ‎2023-09-22 06:48 AM

APC transfer switch UTS10BI circuit 9 & 10 for 240V

My question is around circuit 9 &10 in the switch that need to be connected to a 240V 20A circuit to provide power to the switch during regular operation. Since I do not have a 240V 20A circuit in my main panel the 
electrician will have to add such a breaker there. But since I do not have an existing 240V circuit I would lose these circuits as far as backup through the switch. 
My thought to be able to utilize these was to install a subpanel and pull a couple of 15A and/or 20A 120V circuits from the main panel there to be powered by this 240V 20A circuit. Can the legs from this 240V circuit power a few 120V circuits in the subpanel in a way so it still looks like a 240V circuit to the switch?
 
I understand that the 240V 20A 2P breaker in the main panel would trip the whole subpanel if it tripped but I was planning to move 2-4 120V circuits from the main panel that never pull more than 1-2 A each so do not think it ever would be a problem for the reason of overloading.
 
This 240V circuit in the main panel would be un-balanced but would the UTS care about that?
Attachments
Labels
  • Labels:
  • Universal Transfer Switch
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.