Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-03 08:01 AM
I'm a rank newbie at using a UPS and the associated PowerChute Software but have successfully configured my APC BackUPS 1500VA to shutdown my PC after a 3 minute delay on loss of power. Also plugged into the battery side of my UPS are my wifi router, modem and leak detection system. The problem I discovered today when I tested it by unplugging the UPS from the wall is that shortly after the PC shutdown command is issued and the computer fully powers down within a minute the UPS also turns off and cuts power to the other hardware. Upon shutdown of the PC the UPS was still showing ~50min of run time and as soon as the PC turned off the number started climbing and seemed to stabilize around 180 min so this wasn't a low battery power issue... Is there a setting I'm missing that can change this behavior? Having that leak detection setup still be able to notify me if it detects water would be some nice peace of mind even if the UPS is only giving me another 3 hours of run time.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-04 04:26 AM
The lower end models do not have an option to initiate a graceful shutdown and keep the other loads powered.
The best you can do is buy another low end unit and manage just the PC.
Purchase a higher end unit that allows load shedding / timed outputs.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-04 04:26 AM
The lower end models do not have an option to initiate a graceful shutdown and keep the other loads powered.
The best you can do is buy another low end unit and manage just the PC.
Purchase a higher end unit that allows load shedding / timed outputs.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-05 07:37 AM
I suspected that might be the case. Thanks for the reply!
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.