Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84823members
354277posts

Symmetra PX 40

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
Beekeeper_apc
Crewman
Crewman
0 Likes
2
175

Symmetra PX 40

This was originally posted on APC forums on 5/30/2015


Is the Static Switch module, P/N SYSW40KF hot swappable with the load remaining on the UPS as is normal?

I know the identity board has to be changed to the replacement Static Switch, but can you replace the Static Switch module like you would a redundant Power Module?

Thanks,

JS

Tags (4)

Accepted Solutions
Beekeeper_apc
Crewman
Crewman
0 Likes
0
175

Re: Symmetra PX 40

This was originally posted on APC forums on 6/1/2015


Angela,

Thank you for the fast and informative reply.

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
176

Re: Symmetra PX 40

This reply was originally posted by Angela on APC forums on 6/1/2015


Hello,

I'd definitely recommend verifying this with your local 3 phase support team via email or phone if this is not being done by APC or an authorized service provider, but what I found was:

Static Switch Modules on the Symmetra PX 80 and 100 may be hot swapped. This procedure is not possible on the Symmetra PX 40 and ISX 20K All-in-one.  In some cases, the static bypass feature may still be available even though the SSW is reporting as failed. If the alarm is one of the three listed below then static bypass is available through the Power view (on MIM v17.0 >).

1. Overload in PSU (Severity Level 2)
2. Fan_Fault (Severity Level 2)
3. Heatsink over temp (Severity Level 2)
 
If the SSW fault is on a PX40 and not one of the three alarms listed above then a shutdown will be required to change the SSW.
Beekeeper_apc
Crewman
Crewman
0 Likes
0
176

Re: Symmetra PX 40

This was originally posted on APC forums on 6/1/2015


Angela,

Thank you for the fast and informative reply.