Camera view

Surveillance
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
  • EcoStruxure IT Help Center
  • EcoStruxure IT Help Center Categories
  • Data Center Expert
  • Monitoring NetBotz Appliances in DCE
  • Surveillance
  • Camera view
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • EcoStruxure IT Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

EcoStruxure IT Support

Submit a support request for additional assistance with EcoStruxure IT software.

Request Support
Back to Surveillance
Start a Topic
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
920 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Camera view

Picard EcoStruxureIT
‎2019-11-20 06:13 AM

 
 

Camera view

Displays a real-time view of the camera feed along with information about the selected NetBotz Appliance.
The Camera view consists of two areas, the displayed real-time feed from the selected device, and a Camera Information area.The Camera Information area contains Pod Label, Camera Label, Hostname, Location, Status, Licensed, Model, and Device Groups information for the camera.The following icons are located on the upper right-hand side of the view:
Icon Description
92307555_360038795394.png92307555_360038795394.png Click this Listen icon to hear the accompanying audio stream for the selected device.

Note

 

Disabled when no audio is available.

92307554_360038795394.png92307554_360038795394.png Click this Talk icon to send audio to be played at the device.

Note

 

This feature is only available on certain models and requires a microphone on the user's side, and a set of external speakers on the device side.

92307553_360038795394.png92307553_360038795394.png Click the chevron associated with this Change Resolution icon to select the resolution you want to use to display the real-time feed for the selected camera.
92307552_360038795394.png92307552_360038795394.png Click this Retrieve Clips icon to view, tag, export, and delete existing surveillance clips.
You can use the right-click menu in the real-time feed area to do the following:
  • Access the "Recorded Camera Clips" display to retrieve, view, and tag clips for the camera (Retrieve Clips option, or use the 92307552_360038795394.png92307552_360038795394.png icon).
  • Access the "Surveillance Settings" display to configure the camera (Surveillance Settings option).

    Note

    Surveillance Settings in the Device menu allows you to configure cameras for all device groups; Surveillance Settings in the Device Groups view allows you to configure cameras for a selected device group; Surveillance Settings in the Thumbnails view allows you to configure selected cameras for a selected device group.

  • Access the "Device Launch Settings" display to define the settings used to access the web interface at the camera's NetBotz Appliance (Device Launch Settings option).
  • Launch to the web interface at the camera's NetBotz Appliance (Launch to Device option).
  • Log on to the Advanced View interface at the camera's NetBotz Appliance (Launch Advanced View option).

    Note

    This option is enabled by Advanced View Settings, a Client Preferences option in the File menu.

  • View the Device View listing for the camera in the Monitoring perspective (Show in Monitoring Perspective option).
  • Access the "Camera Settings" display to configure the camera at the monitored NetBotz Appliance (NetBotz Appliance Camera Settings option).

Two-Way Audio

When connected to a device capable of capturing and broadcasting sound, you can transmit sounds to and from the device through the server.

You can use the Camera view controls to stream audio from camera pods that have microphones, and to use a microphone connected to your system to send audio to camera pods that have connected speakers.

Note

For two-way audio to work, the camera must be able to connect directly to the client on a public accessible network.

  • To listen to streaming audio from the currently selected Camera Pod (if available) click the 92307555_360038795394.png92307555_360038795394.pngbutton.

    Note

    More than one client can listen to the audio stream simultaneously.

  • To transmit audio from your system to speakers that are connected to the selected Camera Pod, click the 92307554_360038795394.png92307554_360038795394.png button while speaking into your system's microphone.
  • Audio is transmitted only while the 92307554_360038795394.png92307554_360038795394.png button is depressed.
  • While the 92307554_360038795394.png92307554_360038795394.png button is depressed you will not be able to hear audio that is streaming from the target Camera Pod.
  • While the 92307554_360038795394.png92307554_360038795394.png button is depressed it will lock the audio transmission so only your client can send audio to the selected camera pod.
 
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.