Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

new Revox Application available

SpaceLogic KNX Forum

Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
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
  • EcoStruxure Building
  • Light and Room Control
  • SpaceLogic KNX Forum
  • new Revox Application available
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Thomas_Rohde
Sisko Thomas_Rohde Sisko
132
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
60
Heribert_Dölger
Commander Heribert_Dölger Commander
31
View All

Recommended Forums

  • Intelligent Devices Forum

  • SmartConnector Forum

  • Metering & Power Quality

Related Products
product field
SpaceLogic KNX - 4ʺ Touch Unit
product field
KNX Push Button Dynamic Labeling, universal
product field
Wiser for KNX : logic controller

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to SpaceLogic KNX Forum
Start a Topic
PetrMares
Commander PetrMares Commander
Commander

Posted: ‎2020-03-24 01:26 AM . Last Modified: ‎2024-07-14 11:48 PM

1 Like
0
942
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
‎2020-03-24 01:26 AM

new Revox Application available

Let me inform you that we have just released Revox Application together with an Application note. The application has been created by Revox company which is a leader in audio system technologies.

https://www.revox.com/

 

Note: The application is available (visible in marketplace) for controllers running on imx6 CPU (hw2.0 and newer).

 

Desriptions:

 

EN

Control your Revox Multiuser system from a web based application. The application scans your network and the server with all connected Multiuser amplifier are added automatically. You can control all the features like play, pause, next, previous,volume, playlist selection, favorite list and playlist configuration. The applications automatically loads all items available in Revox system. The application can create a widget for controlling a zone, for selecting sources and selecting users (up to 8 user) to control the Revox Multiuser system from the Touch.

 

GE

Steuern Sie Ihr Revox Multiuser-System über eine webbasierte Anwendung. Die Anwendung durchsucht Ihr Netzwerk und der Server mit allen angeschlossenen Multiuser-Verstärkern wird automatisch hinzugefügt. Sie können alle Funktionen wie Wiedergabe, Pause, Nächste, Vorherige, Lautstärke, Auswahl der Wiedergabeliste, Favoritenliste und Konfiguration der Wiedergabeliste steuern. Die Anwendungen laden automatisch alle im Revox System verfügbaren Elemente. Die Anwendung kann ein Widget zur Steuerung einer Zone, zur Auswahl von Quellen und zur Auswahl von Benutzern (bis zu 8 Benutzer) zur Steuerung über den Touch erstellen.

 

 

FR

Contrôlez votre système Revox Multiuser via une application Web. L'application recherche votre réseau et le serveur avec tous les amplificateurs multi-utilisateurs connectés est ajouté automatiquement. Vous pouvez contrôler toutes les fonctions telles que lecture, pause, suivant, précédent, volume, sélection de la liste de lecture, liste des favoris et configuration de la liste de lecture. Les applications chargent automatiquement tous les éléments disponibles dans le système Revox. L'application peut créer un widget pour contrôler une zone, sélectionner des sources et sélectionner des utilisateurs (jusqu'à 8 utilisateurs) pour un contrôle tactile.

 

 

IT

Controlla il tuo sistema Revox Multiuser tramite un'applicazione web. L'applicazione cerca la tua rete e il server con tutti gli amplificatori multiutente collegati viene aggiunto automaticamente. Puoi controllare tutte le funzioni come riproduzione, pausa, successivo, precedente, volume, selezione della playlist, lista dei preferiti e configurazione della playlist. Le applicazioni caricano automaticamente tutti gli elementi disponibili nel sistema Revox. L'applicazione può creare un widget per controllare una zona, selezionare le fonti e selezionare gli utenti (fino a 8 utenti) per il controllo tramite tocco.

 

  • Thumbnail of SpaceLogic KNX - 4ʺ Touch Unit
    SpaceLogic KNX - 4ʺ Touch Unit
  • Thumbnail of KNX Push Button Dynamic Labeling, universal
    KNX Push Button Dynamic Labeling, universal
  • Thumbnail of Wiser for KNX : logic controller
    Wiser for KNX : logic controller
View products (3)
Attachments
Labels
  • Labels:
  • Information
Tags (5)
  • Tags:
  • application
  • application note
  • fellerLYnk
  • spacelynk
  • wiser for knx
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.