Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Search in
Link copied. Please paste this link to share this article on your social media post.
Dear Team, I wanted to add voice control functionality, but I'm not able to connect to the built in app store (Start page > Configure apps) and update previously installed apps or install new ones. I can connect to the device remotely through VPN, so it has internet access. Is there any special setting needed for the router? Or is there in an issue with the device?
BR Miklos
Link copied. Please paste this link to share this article on your social media post.
Hello @miklosbakos
Please check your network settings.
As any other device connected to the internet, your controller requires:
- a valid IP address,
- the subnet mask,
- the default gateway IP address and
- the DNS IP address
Link copied. Please paste this link to share this article on your social media post.
As I mentioned even from the local wifi router and also remotely through vpn (von server set up in the router) the built in webserver available. So those 4 settings are correct. Any further suggestions? I receive time to time (maybe werkly basis) a reminder email from Schneider Cloud that the connection lost with the w4knx, so even with the schneider cloud the device can communicate, I am sure you can see the device in your (Schneider) system. Any further idea please? Or is there any screenshot I should share with you to better understand the situation?
Link copied. Please paste this link to share this article on your social media post.
Hi @miklosbakos
Checking your controller we see it's not connected and we're not able to see which FW version you have installed. Additionally, as shown in the screenshot, the PLugins you have installed are quite old and will need to be updated.
Checking with our CC, they also told me the error message you see is sown when you have no internet connection, bad DNS settings of the controller, and that sometimes helps to clear browser cache. Please try this, clear your cache and check again. if you don't yet have FW version 3.0 installed, please install it and this might also help.
If this is not solved, then please write us back with an update of what you have done.
thanks
Fernando
Link copied. Please paste this link to share this article on your social media post.
Hi Fernando,
1) FW version: 3.0.0
2) Cloud connector tries to reconnect every 30sec based on the Logs
3) If you let me know the Cloud server IP I can try to ping it inside the Network Utilities
4) I attached the eth0 settings, but as I can remotely connect to the local network it shows me there is internet connection, maybe there is special port I have to open in the router?
5) Plugins are old, of course, because the device cannot connect to the internet, that's the main issue we are facing in this ticket.
BR
Miklos
Link copied. Please paste this link to share this article on your social media post.
Hello Miklosbakos!
I am not a network specialist but I wonder about your Router-IP (Default-GW) within the section DNS Server 1?
In the picture below on the right side you see my settings.
Also can you please check if you can reach google succesfully?
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.