SpaceLYnk Lua script If then else

SpaceLogic KNX Forum

Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
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
  • EcoStruxure Building
  • Light and Room Control
  • SpaceLogic KNX Forum
  • SpaceLYnk Lua script If then else
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Thomas_Rohde
Sisko Thomas_Rohde Sisko
132
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
60
Heribert_Dölger
Commander Heribert_Dölger Commander
31
View All
Related Products
product field
SpaceLogic KNX - 4ʺ Touch Unit
product field
KNX Push Button Dynamic Labeling, universal
product field
Wiser for KNX : logic controller

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to SpaceLogic KNX Forum
Start a Topic
Anonymous user
Not applicable

Posted: ‎2015-11-23 02:54 AM . Last Modified: ‎2024-07-14 11:57 PM

0 Likes
3
1138
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
‎2015-11-23 02:54 AM

SpaceLYnk Lua script If then else

Hi

I don't know anything about scripting and I need some help .

I have a KNX project which has a temperature sensor which can only send "ON(1)" or "OFF(0)", and a heat actuator which can only recieve 0-100%(0-255).

We can't change the equipment.

So what I need is a script and a description on how to :

Bring the ON-OFF signal in to the script

Convert the signal into a 0-255 signal, something like "if 1 then 255 else 0"

And then send the converted signal to the actuator

This way the actuator will go to 100% when getting a "ON" signal from the temperature sensor and go to 0% when getting a "OFF" signal.

I tried to do the "learn-by-doing" approach, but after to many script errors I had to give up and ask for help .

Some extra info

The temperature sensor is a roof mounted combination of temperature and movement sensor from esylux. Called EsyLux PD-ATMO 360i/8 T KNX (EP10427213)

And the actuator is Schneiders own KNX Valve drive (MTN6921-0001)

Any feedback or help is greatly appreciated

  • Thumbnail of SpaceLogic KNX - 4ʺ Touch Unit
    SpaceLogic KNX - 4ʺ Touch Unit
  • Thumbnail of KNX Push Button Dynamic Labeling, universal
    KNX Push Button Dynamic Labeling, universal
  • Thumbnail of Wiser for KNX : logic controller
    Wiser for KNX : logic controller
View products (3)
Tags (5)
  • Tags:
  • bacnet
  • knx
  • lua
  • lua_script
  • spacelynk
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 3
olemotor
Commander olemotor Commander
Commander

Posted: ‎2015-11-24 08:15 PM

0 Likes
2
1067
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
‎2015-11-24 08:15 PM

Check out the KNX sub-community for more discussions on spaceLynk and KNX. You may post questions there as well.

Have you considered using the actuators "Forced position" bit input? Using that I believe the actuator can be controlled directly from the thermostat.

Having said that, below is a script example that should do the logic that you request without flooding the bus with write telegrams.

In this example, group 1/1/1 is the thermostats output and 1/1/2 is the actuators input.

inval = grp.getvalue('1/1/1')

outval = grp.getvalue('1/1/2')

if inval == true then

  newval = 255

else

  newval = 0

end

if (newval == 255 and outval < 255) or (newval == 0 and outval > 0) then

  grp.write('1/1/2', newval)

end

Ole Morten
Reply
Anonymous user
Not applicable

Posted: ‎2015-11-24 10:48 PM

0 Likes
1
1067
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
‎2015-11-24 10:48 PM

Hi

Thank you very much for your answer

Yeah I have considered using the forced position, but I am not sure if it will return to its original position when the force position signal goes to 0 again.

It's something I would have to test, was thinking about using the summer  mode bit to close it then.

But you seem to know your way around Lua scripting, is it also possible to make a regulator script. Real value temperature in, setpoint in and a signal between 0-255 out to the valve actuator?

That way it would be much less movement for the valve actuator.

Reply
olemotor
Commander olemotor Commander
Commander

Posted: ‎2015-11-24 11:46 PM

0 Likes
0
1067
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
‎2015-11-24 11:46 PM

Yes it is possible to create PID controls with Lua. So far I have not had the pleasure to test or use this myself. However if you search the web you will see various solutions. Here is a very good example for a quite equivalent product that should fit right into the spaceLynk: PID control

Ole Morten
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.