Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

ETS Program for MTN6354-0019

SpaceLogic KNX Forum

Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
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
  • EcoStruxure Building
  • Light and Room Control
  • SpaceLogic KNX Forum
  • ETS Program for MTN6354-0019
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Thomas_Rohde
Sisko Thomas_Rohde Sisko
132
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
60
Heribert_Dölger
Commander Heribert_Dölger Commander
31
View All

Recommended Forums

  • Intelligent Devices Forum

  • SmartConnector Forum

  • Metering & Power Quality

Related Products
product field
SpaceLogic KNX - 4ʺ Touch Unit
product field
KNX Push Button Dynamic Labeling, universal
product field
Wiser for KNX : logic controller

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to SpaceLogic KNX Forum
Start a Topic
Solved
TECHMECH
Crewman TECHMECH
Crewman

Posted: ‎2022-05-23 06:10 AM . Last Modified: ‎2024-07-14 11:44 PM

1 Like
1
846
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
‎2022-05-23 06:10 AM

ETS Program for MTN6354-0019

Hi team

 

Need help me on MTN6354-0019 high bay sensor programming. 

 

Problem- In one of the Wearhouse we installed this sensor,  if we use one sensor for one circuit then this is working fine , asper site req, we used 3 sensors for one circuit because no of light fixtures are more. Given the time delay of 3min, in this case once we gave the movement  the load is getting on/off, on/off. its not working properly, some times not taking the movement also. what could be the problem and also need solution. 

 

Is we can configure master /slave configuration in ETS. If yes pls attach the documents ?

 

Waiting for your valuable replay.

 

  

  • Thumbnail of SpaceLogic KNX - 4ʺ Touch Unit
    SpaceLogic KNX - 4ʺ Touch Unit
  • Thumbnail of KNX Push Button Dynamic Labeling, universal
    KNX Push Button Dynamic Labeling, universal
  • Thumbnail of Wiser for KNX : logic controller
    Wiser for KNX : logic controller
View products (3)
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Thomas_Rohde
Sisko Thomas_Rohde Sisko
Sisko

Posted: ‎2022-05-24 02:44 AM

0 Likes
0
805
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
‎2022-05-24 02:44 AM

Hello TECHMECH,

to "Is we can configure master /slave configuration in ETS. If yes pls attach the documents ?"
The master/slave function is pretty easy to handle.
Within a dedicated Light-Channel you find a parameter called "Slave input".
With this paramter you can define how the master/slave function works.

General parameter.png

Selection "Slave input = ON"
Each ON-Value on the slave input will start/retrigger the staircase timer, if the brightness condition is fulfilled.
An ON-Value is the same as a movement detected in front of the detector.
This is the normal function when having other detectors as slaves and it is the same function as the master-trigger object of the Argus.

Setting_ON.png


Selection "Slave input = ON/OFF"
With the slave input set to ON/OFF, then as long as the slave input is ON the staircase timer is permanently retriggered.
Not until the slave input is OFF and there is no movement in front of the detector, the staircase timer will run out.
For example to keep the light on without movement using a time switch or push-button, but still brightness dependent.

Setting_ON_OFF.png

 

Kind regards
Thomas

Application Design Engineer

See Answer In Context

Tags (1)
  • Tags:
  • english
Reply
Reply 1
Thomas_Rohde
Sisko Thomas_Rohde Sisko
Sisko

Posted: ‎2022-05-24 02:44 AM

0 Likes
0
806
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
‎2022-05-24 02:44 AM

Hello TECHMECH,

to "Is we can configure master /slave configuration in ETS. If yes pls attach the documents ?"
The master/slave function is pretty easy to handle.
Within a dedicated Light-Channel you find a parameter called "Slave input".
With this paramter you can define how the master/slave function works.

General parameter.png

Selection "Slave input = ON"
Each ON-Value on the slave input will start/retrigger the staircase timer, if the brightness condition is fulfilled.
An ON-Value is the same as a movement detected in front of the detector.
This is the normal function when having other detectors as slaves and it is the same function as the master-trigger object of the Argus.

Setting_ON.png


Selection "Slave input = ON/OFF"
With the slave input set to ON/OFF, then as long as the slave input is ON the staircase timer is permanently retriggered.
Not until the slave input is OFF and there is no movement in front of the detector, the staircase timer will run out.
For example to keep the light on without movement using a time switch or push-button, but still brightness dependent.

Setting_ON_OFF.png

 

Kind regards
Thomas

Application Design Engineer
Tags (1)
  • Tags:
  • english
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.