Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

5500NAC SetLightingLevel() broken after firmware 1.14.0

SpaceLogic C-Bus Forum

Schneider Electric forum about the C-Bus platform to get support and share knowledge including Network Automation Controller (NAC), Application Controller (AC) at selection, installation and troubleshooting sides.
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
  • EcoStruxure Building
  • Light and Room Control
  • SpaceLogic C-Bus Forum
  • 5500NAC SetLightingLevel() broken after firmware 1.14.0
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
sesa96364
sesa96364 Schneider Alumni (Retired)
9
KCWong
Lieutenant KCWong Lieutenant
4
ZeeZee97
Administrator ZeeZee97 Administrator
1
View All

Recommended Forums

  • Intelligent Devices Forum

  • SmartConnector Forum

  • Metering & Power Quality

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to SpaceLogic C-Bus Forum
Start a Topic
Benny_A
Crewman Benny_A
Crewman

Posted: ‎2023-04-22 08:14 PM

0 Likes
4
1711
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
‎2023-04-22 08:14 PM

5500NAC SetLightingLevel() broken after firmware 1.14.0

SetLightingLevel('Bed 1 WIR', 255, 4) light is ramped on -- can see it all correct,

then call SetLightingLevel() again and nac dosnt update object value correctly.

5500Nac showing Current Value to be 0->255(4sec) after 4 sec it never changes to 255 

5500Nac never changes the Current Value to be 255 even though the light is fully on.

 

also the same occurs when manual controlling the object/group address on the objects tab in the UI with the set value button, when setting a ramp command the first one works but if you attempt to set it to the same level it already is at, it shows the current value to be the ramp command 0->255(4sec),

so nac actually thinks the object value is 0 

 

looking in toolkit application log, the ramp command is sent every time by the 5500NAC but the NAC dose not update the actual level of the Object it shows the current value to be the ramp command 0->255(4sec) and not 255 which is the current value of the object/GA according to toolkit.

 

Seems like something else gets broken on every firmware release.

 

 

 

 

Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 4
DarrenMullighan
Ensign DarrenMullighan Ensign
Ensign

Posted: ‎2023-04-23 11:27 PM . Last Modified: ‎2023-04-23 11:30 PM

0 Likes
1
1651
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
‎2023-04-23 11:27 PM

Hi Ben,

 

I have been attempting to replicate this here, but sadly without success, I get a similar effect when I do not have C-Bus connected to the NAC, but based off your description, it sounds like you have this connected to yours?

 

Are you testing this on objects that were created after the firmware update? or prior to? I would be curious to identify roughly how old the project is that you are testing on here.

 

Any details would be appreciated, thanks

 

Edit: Nevermind, I believe I have just replicated the SetLightingLevel() issue

Reply
Benny_A
Crewman Benny_A
Crewman

Posted: ‎2023-04-25 12:30 PM

0 Likes
0
1638
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
‎2023-04-25 12:30 PM

Hi Darren,

 

Thanks for your reply,

at least I'm not going crazy 😂 and you are able to replicate something,

 

This project has gone through a few changes over the years, started of as a SHAC, one of the earlier ones, which failed, then was replaced with a NAC about 3 years ago the complete project was recreated form scratch when NAC was installed.

 

yep Cbus connected, its hard to explain, but as simple as i can, when the object is already at level 255 and we use setlightinglevel() NAC sends the command out but doesn't update its own object after the ramp time so it thinks its still ramping

 

all objects have been created prior to firmware update. 

I'm curious to know if it makes a difference if you do the firmware without a project installed - eg factory default then install firmware - then upload cgl and project backup?

- is there a preferred method for installing firmware or maybe it makes no difference?

Reply
DarrenMullighan
Ensign DarrenMullighan Ensign
Ensign

Posted: ‎2023-04-25 05:09 PM

0 Likes
1
1633
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
‎2023-04-25 05:09 PM

Hi Ben,

 

Firmware updates are designed to consider the current state of the project and update them to work with the new firmware. So the method of updating the firmware without factory defaulting first is the method we recommend.

 

In regards to your logic not reporting back the correct level while it is ramping though, it is possible to use the GetCBusTargetLevel() function to report back the level of the group address that it is intending to go to

 

-- Get target level of application 56 group 1 on the local network
value = GetCBusTargetLevel(0, 56, 1)

Reply
Benny_A
Crewman Benny_A
Crewman

Posted: ‎2023-04-26 04:21 PM

0 Likes
0
1619
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
‎2023-04-26 04:21 PM

Hi Darren,

 

Its not so much the while ramping that's my problem just that if object is already at 255 and you ramp the object to 255 with a ramp rate it never resolves to 255 on the nac object and its status is stuck in the ramping phase even after ramp timeout period. is that what you have observed with testing is it a bug?

 

I can manage a work around with code using if GetLightingLevel() ~= 255 and  GetCBusTargetLevel() ~=255 then ... etc

so that if it is on already or ramping to 255 then another command is not sent
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.