Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Get support to configure, troubleshoot, update or upgrade your motor management solution built with Altivar variable speed drives and Tesys devices to start, control, protect and monitor Low Voltage and Medium Voltage motors and loads, covering direct start, soft start and variable speed control.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-03-20 10:03 PM
Dear Expert,
I have a to choose a VFD for 93KW motor which is connected to the centrifugal pump.
But, i see catalog in which drives are available at 90 KW and 120 KW only.
If i choose 90KW, will I suffer in running the pump or it will run smoothly without any trips?
MOTOR NAMEPLATE
HZ - 50
HP - 125
RPM - 1480
VOLT - 415
FLA - 158
SF 1.15 PF(COSØ)86(0.86)
Thank you.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-03-21 03:59 AM
This application, with this power will require an ATV600. The next topic as you mention is the power selection, as you say, normally the way is to choose power just above your motor power (in your case could be ATV630D90N4). Another criteria has to be taken in account is the motor FLC (full load current), here you mention 158A, then you check the max permanent current is 173A (lower than what you need). D90 is convenient.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-03-21 03:59 AM
This application, with this power will require an ATV600. The next topic as you mention is the power selection, as you say, normally the way is to choose power just above your motor power (in your case could be ATV630D90N4). Another criteria has to be taken in account is the motor FLC (full load current), here you mention 158A, then you check the max permanent current is 173A (lower than what you need). D90 is convenient.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.