Ask our Experts
Didn't find what you are looking for? Ask our experts!
Search in
NMC Support
Submit a support request for additional assistance with EcoStruxure IT software.
Link copied. Please paste this link to share this article on your social media post.
| Component | File | Details |
| Smart-UPS Ultra Application | apc_hw21_sucan_2-5-1-3.nmc3 | UPS Application for Smart-UPS Ultra 5-20 kW. |
For details on upgrading the UPS Network Management Card 3 (NMC 3) firmware, see the NMC3 User Guide.
|
New Feature |
UPS Family | |
| SRTL Devices | SRYL Devices | |
| Support added for Dell VxRail. | ♦ | ♦ |
| Support added for new Smart-UPS Ultra devices SRTL8KRM4UI and SRTL10KRM4UI, both devices have Switched Outlet Groups. | ♦ | ♦ |
| Display screen improvements. See the Fixed Issues section for more details. |
♦ | |
| Support added for Smart-UPS Modular Ultra devices SRYL13KRMM and SRYL18KRMM. | ♦ | |
| The NMC now supports UPS firmware updates while the UPS is in Manual Bypass mode. | ♦ | |
| The system now allows the setting of Output Voltage when the output is in Manual Bypass. | ♦ | |
|
Fixed Issue |
UPS Family |
|
|
SRTL Devices |
SRYL Devices |
|
|
The data log values were updated for kW and kVA. |
♦ |
♦ |
|
You can now set the Output Frequency Slew Rate from the Web UI. |
♦ |
♦ |
|
Always acceptable and Never acceptable options were added in SNMP to the upsAdvConfigBypassPhaseLockRequired OID. |
♦ |
♦ |
|
The location of internal battery modules are now also displayed in the Web UI. |
♦ |
♦ |
|
UPS firmware upgrades work as expected if initiated via the NMC in the SmartSlot. |
♦ |
♦ |
|
The UPS Event Log now displays battery frame information when battery modules are removed or installed. |
♦ |
♦ |
|
The NMC now supports the latest set of UPS alarms with the correct severity. |
♦ |
♦ |
|
The default baud rate was changed to 9600 for UIO serial port |
♦ |
|
|
The NMC no longer reports lost communications for 30-50 seconds. |
♦ |
|
|
The Power Module Fault message now includes the faulted power module location. |
|
♦ |
|
The NMC and its display will now reboot after performing ‘Reset all Exclude TCP/IP’. |
|
♦ |
|
After setting the IP address manually via the display, the NMC and its display now reboots automatically as expected. |
|
♦ |
|
The UPS status is now correctly shown in the display when the UPS is in Software Bypass and Temporary Bypass modes. |
|
♦ |
|
When the UPS is in Error condition, the UPS status now correctly reports the Error state on the display. |
|
♦ |
|
Saving the Debug Log on a USB drive will now provide the full set of files as expected. |
|
♦ |
|
Line-to-Line output voltage is now reported in the NMC data log. |
|
♦ |
|
The reported load percentage on the display’s home screens is no longer dependent on the redundancy setting and always uses the N+0 value. |
|
♦ |
|
When the display access is disabled, the user cannot log in on the display. |
|
♦ |
|
The Status > UPS > Output screen on the display has been updated to always show the percent power values at N+0 regardless of the redundancy setting. |
|
♦ |
|
The minimum to maximum range data has been removed from the display configuration screens. |
|
♦ |
|
When the UPS is off without an error condition, the display will now show ‘Output Off’ as expected. |
|
♦ |
|
The Status > UPS > Overview screen on the display is now redesigned for localization support. |
|
♦ |
|
On the display, the USB menu will now show as expected after |
|
♦ |
|
Following a successful UPS firmware upgrade via a USB drive, USB-related options under the Configuration > USB screen are now available in the display. |
|
♦ |
|
The CLI now allows you to change the redundancy alarm setting via cfgpower -red command. |
|
♦ |
| Known Issue | UPS Family | |
|
SRTL Devices |
SRYL Devices |
|
| After updating the NMC’s firmware via a USB flash drive, the USB is not recognized in the display or NMC Web UI. | ♦ | ♦ |
| Some pages in the Web UI help are not updated. | ♦ | ♦ |
| It can take up to 30 minutes to complete a UPS firmware upgrade when using HTTPS. To workaround this, use SCP as an alternative. | ♦ | ♦ |
| The alarm description is shown incorrectly in DCE for outlet group-related alarms. | ♦ | |
| You cannot unzip the debug file completely from a USB drive. This issue is seen intermittently. | ♦ | |
| When a UPS firmware upgrade is in progress, the upsAdvcontrolFirmwareUpdate SNMP OID incorrectly reports the value as “noFirmwareUpdate” instead of “UpdateinProgress”. |
♦ | |
| Filtering by time does not work for the Power Event Log. | ♦ | |
| Entering unsupported commands in the Command Line Interface (CLI) does not return a E102 Parameter error. | ♦ | |
| You are unable to configure some OIDs upsAdvConfigAlarmRedundancy, upsAdvConfigHighBypassLLTransferVolt, upsAdvConfigLowBypassLLTransferVolt from SNMP interface. |
♦ | |
| Only alphanumeric passwords are supported for new users created in the NMC for access to the display. | ♦ | |
| When an internal or external Battery Module is connected or disconnected from its slot, the Event Log entry does not report its serial number. | ♦ | |
| You cannot make configuration changes via the display when RADIUS is enabled and the User Mode is set to “Authentication Needed”. | ♦ | |
| The option to cancel or mute a UPS audible alarm is not present in the Web UI. | ♦ | |
| The ups -s start CLI command is unsuccessful even when the self-test is started correctly. | ♦ | |
| There is no option to set the language of the display in the NMC Web UI. | ♦ | |
| There is no option in the Web UI or the display to cancel a UPS audible alarm test. It is not recommended to initiate a continuous alarm as the only way to stop the UPS beeping is to turn off the UPS. | ♦ | |
| You cannot modify the output voltage setting from the SNMP interface if the output is in Manual Bypass. | ♦ | |
| The “Minimum Redundancy lost" event is not displayed in PowerChute Network Shutdown although it is supported by the NMC. If this event occurs, the server will not shutdown. | ♦ | |
| Signatures | apc_hw21_sucan_2-5-1-3.exe |
| CRC32 | 2B309B2E |
| CRC64 | DF6A37B237A23FC4 |
| SHA-256 | 0E6A13148CBD3EF5C860A7FA11713B3BB3416B0FF0DD8F59E613ACEC0D2A4FFB |
| SHA-1 | C54FA1BA2349383C3FB9FABBEE752C534804F868 |
| BLAKE2sp | 98F421FE6BF7823CA77518E42E557E84EA3D0F97DAEBFB74AFA8E7882237CCFA |
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.