Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84475members
353691posts

Wiser - Pairing the Unica connected Universal push button dimmer

Schneider Electric Wiser Forum

Connect with Wiser Smart Home solution experts in the Schneider Electric Wiser forum. Discuss tips on features, updates, installation, and how to get the most out of your Wiser products.

Solved
Esperanto
Lieutenant JG
Lieutenant JG

Wiser - Pairing the Unica connected Universal push button dimmer

Hello, 

 

How can I pair my Connected Universal push button dimmer?

Tags (1)

Accepted Solutions
Alfred_SE
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
1
270

Re: Wiser - Pairing the Unica connected Universal push button dimmer

Hello, thank you for your question
. You can pair the device manually:
Follow the steps to pair the device manually:

  1. On Home page, tap + icon.
  2. Tap the dimmer icon and select the Wiser Hub.
  3. Select any one of the options to add device (A):
  • Add Device with Install Code
  • Add Device without Install Code

Capture.PNG
6. To add the device with Install Code, tap Add Device with Install Code button to open the slide-up menu. Select any one of the options (B):

  • Scan Install Code - You can scan the device for the Install Code
  • Enter Install Code Manually - You can manually enter the install code from the device

After adding the device with Install Code, proceed to Step 6.
Capture.PNG

TIP: It is recommended to add the device with Install Code for security purpose.
5. To add the device without Install Code, tap Add Device without Install Code.

6. Short press upper part of the push button 3 times (< 0,5 s) on the device.
Capture.PNG
The LED blinks amber
7. In the app, select Confirm LED is blinking amber and tap Start configuration (C)
Capture.PNG

The app displays the progress of connecting the device
8. Wait for a few seconds until the device is connected and the app shows that the device is added successfully.

The stable green LED on the Dimmer shows that it is successfully connected to the Gateway


Capture.PNG
9. 
After the device is added in the app, tap Done.









Alfred Francis

See Answer In Context

Tags (1)
Alfred_SE
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
269

Re: Wiser - Pairing the Unica connected Universal push button dimmer

You can also pair the device with auto scan:
Pairing the device with auto scan automatically discovers the device when the corresponding device is powered on.

Follow the steps to pair the device:

  1. On the Home page, tap + icon.
  2. Tap Auto scan tab and tap Confirm.
  3. If you have multiple hubs, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the Wiser hub from the slide-up menu.
  5. Short press upper part of the push button 3 times (< 0,5 s).

NOTE:

  • The LED blinks amber.
  • Wait for a few seconds until the device search is complete.

    6.Tap Push Button Dimmer and tap Next (A).
    Capture.PNG
    7. Once the device is added successfully, tap Done.
Alfred Francis

See Answer In Context

Tags (1)
2 Replies 2
Alfred_SE
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
1
271

Re: Wiser - Pairing the Unica connected Universal push button dimmer

Hello, thank you for your question
. You can pair the device manually:
Follow the steps to pair the device manually:

  1. On Home page, tap + icon.
  2. Tap the dimmer icon and select the Wiser Hub.
  3. Select any one of the options to add device (A):
  • Add Device with Install Code
  • Add Device without Install Code

Capture.PNG
6. To add the device with Install Code, tap Add Device with Install Code button to open the slide-up menu. Select any one of the options (B):

  • Scan Install Code - You can scan the device for the Install Code
  • Enter Install Code Manually - You can manually enter the install code from the device

After adding the device with Install Code, proceed to Step 6.
Capture.PNG

TIP: It is recommended to add the device with Install Code for security purpose.
5. To add the device without Install Code, tap Add Device without Install Code.

6. Short press upper part of the push button 3 times (< 0,5 s) on the device.
Capture.PNG
The LED blinks amber
7. In the app, select Confirm LED is blinking amber and tap Start configuration (C)
Capture.PNG

The app displays the progress of connecting the device
8. Wait for a few seconds until the device is connected and the app shows that the device is added successfully.

The stable green LED on the Dimmer shows that it is successfully connected to the Gateway


Capture.PNG
9. 
After the device is added in the app, tap Done.









Alfred Francis
Tags (1)
Alfred_SE
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
270

Re: Wiser - Pairing the Unica connected Universal push button dimmer

You can also pair the device with auto scan:
Pairing the device with auto scan automatically discovers the device when the corresponding device is powered on.

Follow the steps to pair the device:

  1. On the Home page, tap + icon.
  2. Tap Auto scan tab and tap Confirm.
  3. If you have multiple hubs, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the Wiser hub from the slide-up menu.
  5. Short press upper part of the push button 3 times (< 0,5 s).

NOTE:

  • The LED blinks amber.
  • Wait for a few seconds until the device search is complete.

    6.Tap Push Button Dimmer and tap Next (A).
    Capture.PNG
    7. Once the device is added successfully, tap Done.
Alfred Francis
Tags (1)