New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Modscan to 651 Recloser
Protection & Control
Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
2024-05-3001:49 PM
Modscan to 651 Recloser
I couldn't figure out which board to post so apologies if wrong board
For 651R, there is currently one tcp connection to source port 50018 to port 502 (see attach screenshot). If another tcp connection with modscan with source port 64623 to port 502, it fails. Wireshark shows modscan try 3 times with SYN and fails. However, with other TCP ports such as http (port 80), multiple simultaneous connections are ok. For port 502, it is only limited to one connection at a time?
On manual, I see below so not sure if this is the case.
The TCP port number is the Modbus TCP registered port 502. Modbus TCP uses the device IP address as the Modbus identifier and accesses the data in the relay through use of the same function codes and data maps as Modbus RTU.....Modbus RTU is a binary protocol that permits communication among a single master device and multiple slave devices. The communication is half duplex—only one device transmits at a time