Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hello Team.
Can the Easergy P5 protection relay be used in single-phase 3-wire?
I attach a photo below.
In addition, please check whether it is possible in PM5560.
Link copied. Please paste this link to share this article on your social media post.
Hello Hyeontae-Song,
from the photo it looks like a 3-phase application, may be with just 2 phase CTs ("2-CT").
Such application is feasible/possible with P5F30.
PM5560 I can't comment on.
Regards
Rudolf
Link copied. Please paste this link to share this article on your social media post.
Hello Hyeontae-Song,
from the photo it looks like a 3-phase application, may be with just 2 phase CTs ("2-CT").
Such application is feasible/possible with P5F30.
PM5560 I can't comment on.
Regards
Rudolf
Link copied. Please paste this link to share this article on your social media post.
Thank you for your reply.
However, single-phase three-wire wiring has different voltage levels.
Look at the picture below.
I know that the protection relay is measured on a 3-phase basis.
Link copied. Please paste this link to share this article on your social media post.
I would call this a 2-phase 3-wire application, where the red wire is ground/earth, and blue/black are phase wires with voltages 180° phase shifted.
Is it railway/ metro application?
If yes, then I would check for any railway specific requirements (in terms of functionality and hardware requirements; and also frequency - is 50 or 60 Hz?).
If no, and as no directional protection function is required per SLD (it shows just 50/51 phase OC and 51G neutral OC based on measured IN), then use of P5 would be feasible.
What is the purpose of "Ao" input?
Device power supply will be from 110 V AC? Which is ok from PSU input range, but bears the risk that the relay will power down during a short-circuit on the primary system, then cannot provide reliable protection. A so-called self-powered relay then would be more suitable (like MiCOM P115 or P116).
regards
Rudolf
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.