Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hello everyone,
I would like to address to you in order to get pretender documentation and certificates for Arc flesh protection.
What I would like to get is official certificate or SE document that states what is the time for arc flesh detection for ARC relays. All in order to put it in tender specification.
For example Vamp 321 2ms arc detection and reacting time, or Easergy P3/P5 2/7ms for integrated arc protection.
Also if there is some other pretender specification mostly ofor any of these 3 relays P3 P5 and Vamp321(with modules) it would be nice to have ti.
Best regards,
Link copied. Please paste this link to share this article on your social media post.
Hi Ivan,
First, thanks a lot for making these inquiries about Arc performance and functional test.
IEC standards give criteria about " how to test" and not about protection's performance. That includes Arc protection as well. But in IEC 60947-9-2 ED1 which is under development and would be published later in 2021, the standard describes the ignition & test duration of an arc-fault in the context of an Internal Arc Control Devices(IACD) performance; this defined condition could help to have a rough idea about Arc performance criteria. In standard, the duration of the arc (for stand-alone or multifunction type IACD) is 10ms. If the relay trip <10ms so it passes the test.
Moreover, I’m going to attach the V321 internal Type Test Certificate including the functional test and its performance. Hope it helps. The report covers standard request and also confirm the table you shared.
Regarding P3/P5 I will follow up on the topic and come back to you.
Do not hesitate to contact me if further clarification is required.
hamed.ershadzadeh@se.com
BR
Link copied. Please paste this link to share this article on your social media post.
Hi,
Once again.
Can someone from marketing department (or any other department responsible for this issue) check if there is some official document from SE or even better from independent laboratory that states time for ARC protection reaction for P3/P5 and Vamp 321 system?
Basically certificate that confirms data in the manuals :
Best regards,
Link copied. Please paste this link to share this article on your social media post.
Hi Ivan,
First, thanks a lot for making these inquiries about Arc performance and functional test.
IEC standards give criteria about " how to test" and not about protection's performance. That includes Arc protection as well. But in IEC 60947-9-2 ED1 which is under development and would be published later in 2021, the standard describes the ignition & test duration of an arc-fault in the context of an Internal Arc Control Devices(IACD) performance; this defined condition could help to have a rough idea about Arc performance criteria. In standard, the duration of the arc (for stand-alone or multifunction type IACD) is 10ms. If the relay trip <10ms so it passes the test.
Moreover, I’m going to attach the V321 internal Type Test Certificate including the functional test and its performance. Hope it helps. The report covers standard request and also confirm the table you shared.
Regarding P3/P5 I will follow up on the topic and come back to you.
Do not hesitate to contact me if further clarification is required.
hamed.ershadzadeh@se.com
BR
Link copied. Please paste this link to share this article on your social media post.
Thank you for this clarification.
This can be helpful in pretendering stage of arc flesh solutions for ongoing and future projects.
Please inform us if new documentation described above or some other documentation comes available.
Also for anything you find for now, like V321 internal Type Test Certificate, please attach it in this topic if possible.
Best regards,
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.