Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-17 12:19 AM
Hello,
I am quite new to Schneider ecosystem, I wanted to know how to use retaintive TON or TOFF timer in Ecostrucx HVAC.
Thanks in advance!!
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-26 08:35 AM
If you could tell me which HMI do you use I could tell you how you could reach your goal.
You could use in ESME HVAC the PULS FB to generate an impuls every 1s. Then you could count up a status variabel which you could link in the HMI to a retain variabel. In the HMI you need to generate a script you write this value at startup back to the PLC
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-18 10:25 PM
Hi Josh1,
Please explain what do you need exactly.
The integrated timer could not be specified as retain.
Did you need a timer which save his PT value also on power off?
Or did you need a timer which would not be reset if IN switches from TRUE to FALSE?
For the second case we would find a solution. For the first case unluckily not.
The retain attribut for GLOBAL VAR in ESME HVAC is not supported.
And did you use TM171O or TM171P or TM172 ?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-22 04:38 AM
Thanks for the reply,
I'm using TM171O, and I want to use retentive timer, Which will start counting from where it left when power to the PLC is off.\
Thanks!
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-22 05:05 AM
Unfortunately this is not possible with TM171O.
What would you reache with this function. Maybe there is a other way to reach the same goal.
If you deeper explain you goul we could find a different way.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-22 06:33 AM
I want a timed process, I will give a certain time and then give start command when the process is completed start command is reset, If this process gets interrupted in between due to power failure or as such, after starting up again that process should resume from where it left before the interruption.
And also I am using one HMI to interface it with plc
Thanks.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-24 10:39 PM
Hi Josh,
In that case I would see to possibilities which could be a soultion.
1. I suspect you use a "longer" time for your process (more hh:mm instead of mm:ss). In that case you could use the internal clock of the TM171O. To calculate the time length calculate with the target var sysclock.* (*= hour,minute,secound....)
2. Which HMI do you use? If you use a SE Harmony or a Proface HMI which is based on the new HMIST6 base you could use retain variabeles on the HMI and transfer them via Modbus to the TM171O. The odler basic HMIs like HMISTO did not support retain variabels.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-25 11:24 PM
Thanks, Bastian,
You are being really helpful, can you please elaborate me on how can I use that second method,
Thanks alot
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-10-26 08:35 AM
If you could tell me which HMI do you use I could tell you how you could reach your goal.
You could use in ESME HVAC the PULS FB to generate an impuls every 1s. Then you could count up a status variabel which you could link in the HMI to a retain variabel. In the HMI you need to generate a script you write this value at startup back to the PLC
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.