Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-04-23 04:04 PM . Last Modified: 2025-04-23 04:18 PM
Hello! I'm having two issues when upgrading the firmware on these two devices using EcoStruxure Automation Device Maintenance:
1. I want to upgrade the BMENOR2200H - X80 Advance RTU module. I added it through the catalog using the commercial reference BME*** (upgraded). I was able to connect and follow all the steps, but it never loads 100% and the following error occurs:
2. The same error occurs if I try to update the BME P58 2040 driver, I manage to connect to the device, but at the time of updating, it charges up to 20% (as seen in the image) and does not update.
I have tried different firmware versions but none are able to load to the target device.
These are the versions I want to install and by device:
All files are downloaded from the update center to the local repository
At the time of download, the rack where the PLC and HMI are located is well energized, there is no electrical problem that prevents the update.
With the PLC I connect via Ethernet through the Modbus TCP detection protocol and for the NOR2200 module I connect from the catalog
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-04-25 06:17 AM
Hi,
To migrate, follow these steps:
Here are the links for the 3.99 file download and the video tutorial showing the steps:
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-04-25 06:17 AM
Hi,
To migrate, follow these steps:
Here are the links for the 3.99 file download and the video tutorial showing the steps:
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2026-06-30 06:32 AM
If the error "Invalid Signature" occurs on the BMENOR2200H, the cause is typically an incorrect system time in the PLC.
To resolve this issue on an M580 PLC, follow these steps:
If the PLC shows an incorrect date or time (as illustrated in the screenshot), simply click one of the Update buttons.
Depending on your needs, you can:
After that you probably have to reboot the PLC and the NOR so they can synchronize the new time
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2026-06-30 08:48 PM
It seems you may have this under control, but worth mentioning the settings for the FW upload are set correctly and you record the password.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.