Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
Search in
Please select a country to continue with beta search.
Posted: 2020-06-04 08:51 PM . Last Modified: 2020-06-04 08:53 PM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-06-04 08:51 PM . Last Modified: 2020-06-04 08:53 PM
Dear Experts,
I have two M580 remotes I/Os panel and CPU panel and I want to connect all by using BMXNRP0200 Fibre Converter modules. In IO panels the backplane is BME XBP 1200, after the CPS3500 at slot "0" I have installed CRA 312 module and then all other IO modules AMI, AMO, DDI & DDO. My question is: at which slot on the backplane I need to insert BMXNRP0200 in IO panels and at which slot in the CPU panel and how I need to make ethernet and fiber connection on the module. It has two ethernet ports up and down and two fibre ports up and down. Which ethernet port (up or down) I need to use to connect with CRA and which fiber port (up or down) I can use to connect with another BMXNRP0200 Fiber Converter installed in another panel. I have attached the snap of configuration where I have CPU panel and two remote IO panels ?
Best Regards,
Ahmed
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-06-08 07:49 AM
Hello @Chao could you help?
Rodrigo G.
Industrial Automation Community manager
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-06-08 09:10 PM
1) BMXNRP module is a simple networking fiber converter without network management functions. The modules do not support communication through the backplane connector. Only the power is supplied from the rack. Therefore, It coudl be installed in any slot on the X80 racks, whatever in local rack of CPU, extended rack, remote IO stations or distributed IO stations.
2) Since it's physical fier converted, eitehr Ethernet port could be used to connect to CRA. Fiber ETH1 port interlinks cooper ETH1 port while fiber ETH2 port interlinks cooper ETH2 port. For more detailed use case and architecture, please refer to it's user manual published on SE.com. Thx!
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.