Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ALTIVAR930 How send command Word from UnityPro

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
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
  • Industrial Automation
  • Modicon PAC Forum
  • ALTIVAR930 How send command Word from UnityPro
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Trinxs1
Trinxs1 Leader
19
YONGHO-KIM
YONGHO-KIM Mentor
10
ciupol
ciupol
9
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Related Products
product field
Schneider Electric
Modicon M340

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Modicon PAC Forum
Start a Topic
n_zelenev
n_zelenev
Explorer

Posted: ‎2023-11-10 10:57 AM

0 Likes
1
1037
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
Posted: ‎2023-11-10 10:57 AM

ALTIVAR930 How send command Word from UnityPro

Friends, please help me, I’m trying to send the CND command Word16bit  (CND-adress 8501) for run Altivar930 word to the frequency converter, through Unity Pro, but I’m new to MODICON, please tell me how I can send the command words to the frequency converter using the RTU modbus, the plc-altivar930 connection is configured ok

Labels
  • Labels:
  • 01. Modicon M340 PAC
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
SEStig
SEStig Contributor
Contributor

Posted: ‎2023-12-03 09:10 PM

0 Likes
0
1004
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
Posted: ‎2023-12-03 09:10 PM

Is there a reason you are using Modbus RTU and not Modbus TCP?

 

If you use TCP then you can use the IO scanner service in the drive (Unit ID 255, start address 0 for length for both read and write)

 

If you have to use RTU then you can give the drive a Serial address (1-247) and use the Comms Scanner service (modbus field address of drive, read start at 12741 for up to 8 length, write address start at 12761 for a length of up to 8).

 

In either case you need to set the drive to have its CMD channel 1 from the desired source (ethernet or modbus serial) and if you want to se the speed from there as well you can either use Combined Channel profile or IO profile if you want a simpler starting procedure.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.