- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-12-11 07:44 AM
I/O Led M262 lit when Ethernet 1 is not connected
Hello,
We are using M262 PLCs for one of our projects. We configure the Ethernet 1 interface with a static IP address, which is used as a service interface. During normal operation, nothing is connected to this interface. However, the red I/O LED is lit. Is there a way to configure the Ethernet 1 interface so that it is not mandatory and the red I/O LED doesn't light up?
Thanks,
JS
Labels
- Labels:
-
Modicon M2xx
Authentication Failed.
- Authentication Ticket Mismatched, failed authentication.
Link copied. Please paste this link to share this article on your social media post.
Replies 0