Ask our Experts
Didn't find what you are looking for? Ask our experts!
Support Forum for HVAC and pumping machines, Modicon M17x and EcoStruxure Machine Expert HVAC software for chillers, AHU, CRAC units for datacenters or process chillers applications - from design, implementation to troubleshooting and more, by Schneider Electric.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-06-20 06:20 PM
Hi,
In the Programming tab -> Project -> Options -> Build events, there are options for running commands.
I'd like to add script to set some register values after the build, such as the date/time of compilation, or the current git branch I am working on.
How would I go about this? Is it possible that I can set both the value in register to be downloaded, as well as the default value in the source files?
Thanks.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-06-21 03:58 AM
Hi,
not sure it is feasible in this way, another idea could be .bat file which will create a file with all the information you need to be saved in the ExtraNOR0 folder.
It will be automatically downloaded in case of Download All and you can create a program in your project which reads this information and show them into a status variable or EEprom parameter.
Clearly this is a solution just for TM172P
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-06-21 03:58 AM
Hi,
not sure it is feasible in this way, another idea could be .bat file which will create a file with all the information you need to be saved in the ExtraNOR0 folder.
It will be automatically downloaded in case of Download All and you can create a program in your project which reads this information and show them into a status variable or EEprom parameter.
Clearly this is a solution just for TM172P
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-06-24 11:13 PM
I was able to do this. I did have encounter some odd behaviour such as if a file of the same name was already in NOR, then it wouldn't copy. I ended up adding the /EXTRAFOLDER:Extra to force it to the file that I generated, for the CLI download. I haven't vetted the USB loading method but I assume that works the same in putting into NOR. Though it seems I'd have to manually add the custom file to the collection of USB files.
Also I was unaware of the pathing of 'sys_FM_READ'; given I was storing in NOR, I needed 'nor:0:/' prefixed.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.