This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-12-2910:09 PM
lxm32cd72n4 Drive _M_Maxoverload issue
Hello Experts..
We are using an LXM32CD72N4 drive with a BMH140 (3-phase servo motor) to lift approximately 500 kg from water as part of an R&D project. The PLC programs are quite basic, involving lifting to a specified height and dropping based on sensor signals. However, the servo runs 2-3 times (occasionally 5-6) before the motor stops automatically without displaying any error messages. There are no signs of stress or overload. The lift operates up to a height of 2-3 meters before gradually stopping. From the SoMove dashboard, we observed that the "_M_Maxoverload" value increases during operation and the motor stops once this value reaches 105 or higher. Could there be a specific reason why this counter is increasing gradually? pls share your thoughts.. incase if i can contact you directly, pls share your details.. Thanks for your support..