Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84532members
353781posts

Speed up your Pre-Sales project quotation with EcoStruxure™ Plant Builder 4.5: Now available on Exchange!

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Rodrigo_Garcia
Administrator Administrator
Administrator

Speed up your Pre-Sales project quotation with EcoStruxure™ Plant Builder 4.5: Now available on Exchange!

Speed up EcoStruxure™ Plant Pre-Sales project quotation


The EcoStruxure Plant Builder is a quotation pre-sales tool that satisfies the needs of each player in the solution selling process.

It is a standalone tool that is always in line with the latest release of EcoStruxure Plant catalog.

Starting from a project specification, the tool proposes and validates a system configuration comprising:

  • PAC modules
  • devices
  • network
  • software

It provides the complete BOM (Bill Of Material) of the full porject with pricing for project bidding, a customized system architecture drawing and a project quotation report.

 

Plant Builder.JPG

 

Rodrigo G. 


Industrial Automation Community manager

1 Reply 1
Omaelk
Administrator Administrator
Administrator
0 Likes
0
877

Re: Speed up your Pre-Sales project quotation with EcoStruxure™ Plant Builder 4.5: Now available on Exchange!

Great news! 😉

 

 

Tags (1)