This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: โ2023-01-1411:40 AM
Controller design for water tank
Can you please help me with this problem please??
Translation:
The main objective of this work is to develop a PID control algorithm for the Arduino, and the adjustment of its parameters. The plant is in this case a water reservoir with a filling pump with a flow Qi and a leakage flow Q1, adjusted by restriction R1.
The system consists of a water tank 0.5 m high and 0.06 m in diameter, fed by a pump whose flow rate is controlled from an analogue signal V [0 ; 10] VDC. The pump equation is given by: ๐1=Kb*V com Kb=0.000025
At the bottom of the tank there is a leakage flow, ๐1, which can be adjusted through the restrictor ๐ 1. The constraint will always have a positive value (R1>0).
1. Write the equation that describes the system assuming as input the control voltage of the pump and output at liquid height; The. Determine the differential equation that describes the behavior of the system; B. Assume a step input to the pump from 0 VDC to 4.5 VDC; รง. Assume that in operation, the tank stabilizes at a level equal to 0.33 m, determine the value of R1; d. Write the system transfer function,