This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2024-04-0605:38 AM
Can you read the system time from the HMI?
Hi all,
Is it possible to read the system time from a HMIGTO2310/2315?
I have the PLC syncing the RTC time to the HMI using the 'Sys.setTime' function and I could just make the HMI display the last PLC variables used to write to that, however there's surely a simple way to read that time that's just been set directly from the HMI?
Ok, so there's no singular system variable I can read to display the whole time in one go, I'll need to read the variables and combine them into the time format I want.
If that's correct, what is the syntax layout for combining the time variables and how can I force desired formats such as 12/24 hour and if the am/pm flag is shown? Same question for the date as well really.