EcoStruxure Geo SCADA Expert 7 | Architectures

Industrial Automation How-to videos

How-to videos on Schneider Electric Industrial Automation products and solutions. In general, these videos help provide a clear demonstration on the best method to accomplish a given task.
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
  • Industrial Automation How-to videos
  • EcoStruxure Geo SCADA Expert 7 | Architectures
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • Configuration and Programming 111
  • How-to & Best practices 45
  • Telemetry 42
  • Communication protocols 23
  • Solution 15
  • SCADAPack 14
  • Cybersecurity 11
  • Training & How to 9
  • Best Practice 9
  • Wireless 8
  • Realift 7
  • Integration 5
  • Licensing 4
  • How to 3
  • Asset Link 2
  • Harmony 2
  • Selection & sizing 2
  • Control Expert 2
  • Flow Computation 2
  • Smart Design & Engineering 2
  • Application Programming 2
  • Vijeo Viewer 1
  • Commissioning 1
  • Webgate 1
  • Industrial device 1
  • telepace 1
  • EcoStruxure secure connect 1
  • How-to 1
  • Utility Knowledge Base 1
  • Modicon PAC 1
  • M340 1
  • Vijeo Designer 1
  • troubleshooting 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • How to size your solar installation with Altivar Solar Sizer?
  • How to reduce harmonics with passive filter on ATV600, ATV900?
  • How to Configure Flowmeter Function on Altivar Solar ATV320?
  • How to Configure Pulse Counter Function on Altivar Solar ATV320?
  • How to use Industrial Device with EcoStruxure Secure Connect?
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Jimi
Commander Jimi Commander
Commander
‎2020-04-17 04:50 AM
1 Like
0
2256
  • Mark as New
  • Mark as Read
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
‎2020-04-17 04:50 AM

EcoStruxure Geo SCADA Expert 7 | Architectures

Originally published on Industrial Automation How-to videos by Jimi | April 17, 2020 01:50 PM

 

This 7th Geo SCADA tutorial video describes the various architectures options that can be implemented with EcoStruxure Geo SCADA Expert, the dedicated SCADA software for remote SCADA & Telemetry applications.

 
Geo SCADA can be set up in a wide variety of architectures to suit your need for redundancy, scalability, networking and plant or asset geographies.
 
- The simplest architecture is a single server connecting to remote devices. Its communication drivers are retrieving data and enabling control because the server is in a mode called ‘Main’. All data is stored on the server, and one or more ViewX clients are displaying that.
 
- Add a second server to enable redundancy. This server is in ‘Standby’ mode. If the first server has failed or stopped, the second takes over data gathering, control and client connections. When the first server is restored, its data is automatically resynchronized and within seconds to minutes it’s ready to go Main when needed.
 
- Add a third redundant server, which is synchronized from the Main server. There are configuration options to control the priority of servers, so you can prefer changeover to A and B over C.
 
- Geo SCADA has built-in configuration features to detect and mitigate undesirable redundant server operation in the event of a network failure.
 
- Clients can be configured to connect and retrieve data from Standby servers. 
 
- By adding more servers (called Performance Firewalls) in a mode called ‘Standby Only’, or ‘Permanent Standby’, they act as synchronized copies of the database. There can be up to four, providing data to hundreds of clients. The built-in historian can be set up for a longer time period of storage for these servers – perhaps 10 or more years. An architecture involving Standby-Only servers would usually incorporate network firewalls, and this provides an architecture which separates control operations from business. There are built-in features in Geo SCADA for controlling the permissible activities from each type of server.
 
- Everything discussed here is part of the Geo SCADA server and client software, and configured with simple screens.

 

 

Never miss any update by watching our full playlist of EcoStruxure Geo SCADA software videos

 

Our experts are ready to answer your questions and technical issue on Geo SCADA Expert forum and SCADA and Telemetry Devices forum 

Labels:
  • Configuration and Programming

  • Solution

  • Telemetry

  • Tags:
  • EcoStruxure Geo SCADA Expert
  • SCADA integration
  • SCADA programming
  • SCADA software
  • SCADA tutorial

Author

Biography

Jimi

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article

Would you like to add a comment?

All registered members have full access to the Community and can post comments and start topics.

  • Sign in / Register
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.