Share Your Feedback – Help Us Improve Search on Community!
Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey
Monitoring operations in Map View
ITA desktop client
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
You can use the map view to monitor the IT Advisors in a quick overview, including any alarms in different locations and rooms. From the map overview, you can double-click to drill down to locations > rooms > racks > servers for details or troubleshooting (and use the Up icon in the Toolbar to drill back up through the location hierarchy).
The Map View is the default view when you launch the application the first time. Subsequently, you can access it by clicking the Map View icon in the Toolbar 102237227_360037995134.png or by double-clicking a location folder in the Navigation pane.
Locations and rooms are represented by information boxes with pins pointing to a location on the map. You can collapse and expand the information boxes by toggling the arrow icon in the upper right corner of the box.
Alarms overview
When collapsed, the information boxes hide the details but have an alarm status icon in the upper left corner. This allows you to see if there are alarms even when the box is collapsed. When expanded, the information boxes show the details, including an alarm section, summing up the total amount of alarms and the amount of normal, warning, critical alarms.
Normal: No alarm conditions exist. Warning: A condition exists that may require attention to ensure it does not deteriorate into a critical state. Critical: A condition exists that requires immediate attention.
When the system receives alarm updates from an external system, the info panel icons will fade in and out.
Capacity overview
If you have a valid IT Advisor: Capacity license, the information boxes also show a capacity overview represented as a pie chart. It sums up the status of power, cooling, space, and network of the selected location or room.
Power is represented as the percentage of the available load (kW) that is utilized by the IT equipment in the location or room. Cooling is represented as the percentage of the available load (kW) that is utilized by the IT equipment in the location or room. U-space is represented as the percentage of the available U-positions (U-pos) that is populated with equipment in the location or room. Network is represented as the percentage of the available Network ports (ports) that is utilized by networking equipment in the location or room.
Note
The amount of ports shown in the capacity overview here may not be the same as you see in the Network overlay of the room layout.
Whereas the floor layout Network overlay shows the amount of ports for racks with network equipment including patch panels, the global capacity overview shows network information represented as a percentage of the available network ports utilized by networking equipment, not including patch panels, in the location or room.
The data is updated on a daily basis by default. If, for some reason, the data is not recorded, for example because the server was turned off, you can re-enable recording in Tools>Preferences>Capacity History by clicking Record Now.
102237230_360037995134.png
123 Steps to...
See also
Creating a geographical representation of the data center infrastructure
Create a representation of locations and rooms.
Select Planning>Data Center in the Application bar to be able to edit.
In Navigation, select the root location icon.
Select File>New and one or more of the available elements. - Location (option to add container elements for geographical enterprise hierarchy) - Sub location - Server Room (option to add room elements for representing white space in the model) - Store Room (option to add space elements for representing store rooms in the model, for example for storing newly arrived servers not yet installed in a server room) - Electrical Room (option to add room elements for representing gray space in the model) - Supporting Infrastructure Space (option to add space elements for representing space outside the rooms in the model, for example for chillers on the roof)
If you do not have the Map View open, double-click a location in Navigation to open it.
Drag the information boxes representing the locations and rooms from the upper left corner into the wanted position on the map.
If you want another background image for the map view, customize it.
Right-click the map view and select Properties.
Click Select Image and browse to an image on the computer or network to import the image as background.
If you want to restore the default image, download the image used here and insert it in the same way as with another image.