Share Your Feedback – Help Us Improve Search on Community!
Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey
Advanced power configuration
ITA Capacity
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Power cable connections between rack PDUs and servers are automatically calculated by default.
Turning off the automatic cable connections allows you to overrule the default settings to manually configure cable connections. This is useful for example when configuring an already running data center with a power configuration that is not the most efficient. Once you have modeled the data center in IT Advisor, you can use the capacity features to identify and optimize the design.
Configuration
Toggling cable connection settings is available in Tools>Preferences>Cable Connection if you have IT Advisor: Capacity installed.
Open Tools > Preferences > Cable Connection.
Define the default power connection setup for a server when it is added to the layout from Genomes. In Cable Connection when moving a server, select Auto calculate cable connection or No cable connection.
Define the default power connection setup for a server when it is added to the layout from another position in the Rack Layout or Navigation. In Cable Connection when moving a server, select Auto calculate cable connection or No cable connection.
102237469_360036714873.png
Usage
When you configure manual cable connections, it is important that you remember that any server you add or move to a rack must be manually connected to a rack PDU immediately. Otherwise, you will see load values that are too high.
If the system does not know about the phase connections, it will assume the server draws the load on all phases in a 3-phase setup and triple the load to ensure the UPS can handle the load.
Note: If you add equipment using the rack advisor functionality in the Installation Requirements pane, cable connections are automatically calculated regardless of the selection of cable connection preferences.