Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Use of RETAINs in HMI programming

HVAC and Pumping Forum

Support Forum for HVAC and pumping machines, Modicon M17x and EcoStruxure Machine Expert HVAC software for chillers, AHU, CRAC units for datacenters or process chillers applications - from design, implementation to troubleshooting and more, by Schneider Electric.
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
  • Industrial Automation
  • HVAC and Pumping Forum
  • Use of RETAINs in HMI programming
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
FedericoM
FedericoM Mentor
119
Bastian_Schmitz
Bastian_Schmitz Champion
64
M_Cervati
M_Cervati Troubleshooter
18
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Related Products
product field
Schneider Electric
EcoStruxure™ Machine Expert - HVAC

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to HVAC and Pumping Forum
Start a Topic
obscuresc
obscuresc
Troubleshooter

Posted: ‎2021-06-03 05:20 PM

0 Likes
2
3788
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
Posted: ‎2021-06-03 05:20 PM

Use of RETAINs in HMI programming

Hi all,

 

I've unsuccessfully been trying to use RETAIN variables within the HMI of a TM172DCLxxx.

Previously, I have tried to create them and tie them to buttons, resulting in the following error;

 

 

 

error G0096:  RTN_XAUTORECOVERPOWER => Init value object not found

 

 

 

This variable previously worked when it was not a RETAIN type, hence scope was correct and no spelling issues. The HMI Properties window also automatically recognised the type, so it was actually finding the variable.

 

I further tried to define some without assigning to buttons; producing a total of three RETAIN variables, resulting in multiple of the following error type;

 

 

 

error A4100: RTN_USIARCONTROLMODE => Retentive vars space exhausted

 

 

 

Following this, I changed the type of two of them to standard variables to reduce the potential use of the retentive space, however the same error as above.

 

Am I missing something regarding their use?

 

Thanks,

Jack

Labels
  • Labels:
  • HVAC
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
SimA
SimA Contributor
Contributor

Posted: ‎2021-06-03 10:37 PM

0 Likes
1
3783
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
Posted: ‎2021-06-03 10:37 PM

As far as I know, the TM172DCL display doesn't have "retain" memory area.  The retain memory area would be an area that would be retained by the battery automatically without any user action.

 

However, the M172 family has was is called eeprom parameters.  Those values are saved in flash memory.  Because the way an eeprom chip works, there is a maximum of write operation in the life of an eeprom cell.  It is around 100 000 write operation per memory cell. To preserve the life of an eeprom chip, the write to an eeprom parameter is not done automatically.  It can be called from the program with the sysWritePar functions (one per data type, int, bool, etc).  This function is smart and only actually writes to the memory cell if the actual value sent to the function is different then the actual value in the eeprom variable.  This prevents a useless write operation to the memory.

 

Another way to write to an eeprom is from an HMI page.  When an eeprom variable is mapped to a data entry object on a page, the value will be written to eeprom memory each time the value is changed by the user.

 

Hope it makes it a bit more clear how it works.

  • Tags:
  • eeprom
  • english
  • hmi
  • M172
  • retain
Reply

Link copied. Please paste this link to share this article on your social media post.

obscuresc
obscuresc
Troubleshooter

Posted: ‎2021-06-03 10:51 PM

In response to SimA
0 Likes
0
3780
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
Posted: ‎2021-06-03 10:51 PM

Ah ok, I didn't realise that normally they would retained via CMOS.

 

I was hoping to avoid the sysWrite method, as I'd have to have a status variable linked to Programming and the overhead you describe.

 

In the HMI editor, can I manage EEPROM Parameters in any scope? For example, page local procedures or using a message? Is this just a feature of the TM172DCLxxx?
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.