Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

M172* writing to BACnet device object instance

HVAC and Pumping Forum

Support Forum for HVAC and pumping machines, Modicon M17x and EcoStruxure Machine Expert HVAC software for chillers, AHU, CRAC units for datacenters or process chillers applications - from design, implementation to troubleshooting and more, by Schneider Electric.
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
  • Industrial Automation
  • HVAC and Pumping Forum
  • M172* writing to BACnet device object instance
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
FedericoM
FedericoM Mentor
119
Bastian_Schmitz
Bastian_Schmitz Champion
64
M_Cervati
M_Cervati Troubleshooter
18
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Related Products
product field
Schneider Electric
EcoStruxure™ Machine Expert - HVAC

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to HVAC and Pumping Forum
Start a Topic
Solved
obscuresc
obscuresc
Troubleshooter

Posted: ‎2024-09-08 09:02 PM

0 Likes
1
1505
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
Posted: ‎2024-09-08 09:02 PM

M172* writing to BACnet device object instance

Hi,

 

I'm using a TM172PDG18R on 668.14 with EcoStruxure Machine Expert HVAC v1.6.0, and am connecting using Yabe v1.3.0.0.

 

I've noticed that on boot of the PLC, the BACnet device object identifier (IEC side) has both the object type and the object instance fields set i.e. the identifier will be set to 33554462, meaning that the object type is 8, the object instance is 30.

 

If I change the device instance via Yabe, Yabe raises an unhandled exception, and the IEC-side device object type goes to 0. The device instance will be successfully changed, and the PLC is visible at the new device instance.

 

Is this behaviour a bug on the PLC or in Yabe? I would not have thought the device object type would be editable over the wire. I have tried to emulate this behaviour using another BACnet client but I was unsuccessful.

 

Thanks.

Labels
  • Labels:
  • HVAC
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
FedericoM
FedericoM Mentor
Mentor

Posted: ‎2024-09-10 03:17 AM

0 Likes
0
1462
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
Posted: ‎2024-09-10 03:17 AM

Hello,

I think it's normal since the Device changed it's own ID.

Note that if you change the Device ID from BMS, you have to store it into EEprom and use it to set it as new Device ID in case of reboot.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
FedericoM
FedericoM Mentor
Mentor

Posted: ‎2024-09-10 03:17 AM

0 Likes
0
1463
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
Posted: ‎2024-09-10 03:17 AM

Hello,

I think it's normal since the Device changed it's own ID.

Note that if you change the Device ID from BMS, you have to store it into EEprom and use it to set it as new Device ID in case of reboot.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.