Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
Search in
Link copied. Please paste this link to share this article on your social media post.
Originally published on Geo SCADA Knowledge Base by Anonymous user | June 10, 2021 04:12 AM
📖 Home Back
It is strongly recommended that systems running on server hardware need to use the Windows Server operating system. Server operating systems are designed for servicing entire systems rather than individual computers or small networks and so are better suited for larger SCADA Server or Web Server systems with more than two clients.
Systems running on desktop hardware should run desktop operating systems such as Windows 8.1 or Windows 10. Desktop operating systems are designed for user interaction on the computer on which they are installed.
Refer to the following table for supported Operating System versions:
| 32-Bit (ViewX client and SCADA Server) | 64-Bit (ViewX client, SCADA Server and Web Server) | |
|---|---|---|
| Desktop Hardware | Windows 10 (Professional and Enterprise editions) Version 1809 and above. Windows 8.1 (Professional and Enterprise editions) |
Windows 10 (Professional and Enterprise editions) Version 1809 and above. Windows 8.1 (Professional and Enterprise editions) |
| Server Hardware | Nil | Windows Server 2019 (Standard and Datacenter editions) Windows Server 2016 (Standard and Datacenter editions) Windows Server 2012 R2 (Standard and Datacenter editions) Windows Server 2012 (Standard and Datacenter editions) |
Use of Geo SCADA 2020 Legacy WebX requires Internet Explorer 11 for web-based operation. The new Virtual ViewX User Interface is accessible from any up-to-date HTML5 browser on various types of desktop, laptop, tablet or large format phone.
Windows 10 versions supported are limited to those within Microsoft's support policy for Pro and Enterprise at: https://support.microsoft.com/en-gb/help/13853/windows-lifecycle-fact-sheet
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.