Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

ClearSCADA 2010 R1.2 Known Issues

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • ClearSCADA 2010 R1.2 Known Issues
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 05:03 PM
0 Likes
0
765
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
‎2021-06-09 05:03 PM

ClearSCADA 2010 R1.2 Known Issues

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 10, 2021 02:03 AM

📖 Home  Back  
Please read the information below prior to installing ClearSCADA 2010 R1.1 for important information on any known issues.

Upgrade


  • When upgrading redundant servers to a newer version of ClearSCADA (ClearSCADA 2010 R2 and later), a problem was found where the Main server checks only the build number of the version running on the Standby and not the Minor version (eg. 6.71). If the Standby server was found to have a lower build number, the connection would be rejected.

So, upgrading from ClearSCADA 2010 R1.2 to any later released versions such as ClearSCADA 2010 R2/R2.1 and ClearSCADA 2010 R3 will fail.
The fix for this issue will be available in the next service pack release for the later versions.

  • When upgrading redundant servers to newer versions of ClearSCADA (ClearSCADA 2010 R2 and later), please ensure that the Configuration Permits feature is turned off. This feature has been removed in later versions. Leaving this feature on and then upgrading causes the upgraded standby server to not synchronise with the main.


  • Users will not be able to view the properties form for objects on an upgraded standby (ClearSCADA 2010 R2 and later) because 'ReadObject' is now processed on the main. This is to ensure that the configuration shown in the form is always the latest version and also to avoid any optimistic concurrency issues.

When trying to open the properties form of an object or edit a document from the client connected to the upgraded standby, an error message will be displayed saying "Error: Cannot proxy request to older server version".

Client Compatibility


  • Mimics created in ClearSCADA 2010 R2 and later cannot be opened from ViewX clients running version ClearSCADA 2010 R1.2 and older. This could cause ViewX to crash. This is due the addition of the default text border and graph key font in the newer versions.


OLE DB Driver


  • When connecting from Microsoft Excel 2007 to the ClearSCADA database using OLE DB Provider for ClearSCADA, the "Save Password in file" option should be enabled. This saves the login details for the connection in a file. Otherwise, the connection will fail with an "Access is denied." error.

  • Using the OLE DB Provider for ClearSCADA to connect to the ClearSCADA database from Crystal Reports is not supported. The connection will fail with a "Logon failed." error message when trying to do so.


Multi-Trace Ad-hoc Trends


Ad-hoc trends with traces from points belonging to other databases in a multi-database system can be created using the "System" identifier in TrendSpec. However, when these trends are displayed in the web client, the trace containing the System identifier will not be displayed. This is because the web client does not support a multi-database system.

KEPServerEX server for ClearSCADA


To ensure that the new KEPServerEX server for ClearSCADA continues to run when the Windows user logs off, the KEPServerEX for ClearSCADA should be configured to run as a service. To do this, follow the steps below.
  • Start the KEPServerEX for ClearSCADA.

  • Go to Tools > Options Menu.

  • In the "Service" tab, enable the check box "Automatically start as a Windows NT service".

Please note that this option will be greyed out and will not be available on Windows 2008 Server, Windows 7 and Windows Vista. For more information, please refer to the Kepware Online Help.
When the KEPServerEX for ClearSCADA is run as a service, shutting down the ClearSCADA server will not shutdown KEPServerEX. It should be shutdown manually (if required) by right-clicking on the Kepware icon in the system tray and selecting "Shutdown KEPServerEX for ClearSCADA".


Incremental Import


  • Cancelling an Import/Import and Merge in ClearSCADA 2010 results in the imported objects having configuration errors on them with error messages displayed saying "Object has been imported but not yet validated". The recommended recovery procedure for this scenario is to delete the objects that have been imported and to perform the import again.

  • When trying to Import/Import and Merge on a redundant pair of machines, it is advisable to perform the import on the Main machine. When importing on the Standby, the configuration needs to be sent to the Main server to be validated and in case of network failure or any other such problems, this would result in the imported objects in the database to have configuration errors on them that can only be cleared by deleting these objects and performing the import again.


Microsoft Query Editor


The new de-reference operator '->' in SQL is not supported in Microsoft Query Editor. Queries using this operator to retrieve information from the ClearSCADA server will not work from Microsoft Excel and will return an error.

Installer


  • On a clean install on Windows 7 and Windows Vista, ViewX will not be able to create a default system when it is first run, unless it is run as Administrator.

In this case, or if there is no server running on the local machine, the ClearSCADA Client control panel applet will be displayed.
  • On a clean installation of ClearSCADA 2010 R2.1, the classes for OPCDA, OPCAE and OPCHDA are not registered. The user would need to open the Client Configuration dialog and click OK on the configured connection for the classes to be registered. This was changed to add support for the Systems.xml file.






Go: Home Back

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.