ClearSCADA 2009 R1.1 Operating System Support

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • ClearSCADA 2009 R1.1 Operating System Support
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
  • Python code to add Historic Export links to Points
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 06:08 PM
0 Likes
0
691
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
‎2021-06-09 06:08 PM

ClearSCADA 2009 R1.1 Operating System Support

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 10, 2021 03:08 AM

📖 Home  Back  
Systems running on servers should use server operating systems such as Windows Server 2003 or Windows Server 2008. Server operating systems are designed for servicing entire systems rather than individual computers or small networks and so are better suited for larger ClearSCADA systems with more than 5 clients.

Systems running on desktop computers should run desktop operating systems such as Windows Vista or XP. Desktop operating systems are designed for user interaction on the computer on which they are installed.

Windows XP and Windows Vista should not be used for servers with more than 2 clients as the TCP/IP security measures in these operating systems can cause significant delays.



32 Bit Operating Systems



ClearSCADA can be installed on computers using the following operating systems:

Windows Vista Service pack 1 (Ultimate and Business editions only)
Windows Vista (Ultimate and Business editions only)
Windows Server 2003 R2
Windows Server 2003 SP1
Windows Server 2003
Windows Server 2008
Windows XP Professional Edition Service pack 3
Windows XP Professional Edition Service pack 2a
Windows XP Professional Edition Service pack 2
Windows XP Professional Edition Service pack 1
Windows 2000 Server SP4.

ClearSCADA also requires Internet Explorer 6 or Internet Explorer 7. Other browsers are not supported.

64 Bit Operating Systems



ClearSCADA can be installed on computers using the following operating systems:

Windows Vista Service pack 1 (Ultimate and Business editions only)
Windows Vista (Ultimate and Business editions only)
Windows Server 2003 R2
Windows Server 2008

ClearSCADA also requires Internet Explorer 6 or Internet Explorer 7. Other browsers are not supported.


Go: Home Back

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.