Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

What is the best way to connect a temperature sensor to an EGX300?

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • What is the best way to connect a temperature sensor to an EGX300?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Kirk Romain_Polette Kirk
117
Guillaume_Evrard
Captain Guillaume_Evrard Captain
59
Randi_Dolan
Commander Randi_Dolan Commander
46
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Gateways and Energy Servers
Start a Topic
maxencevanhove
maxencevanhove Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2014-01-03 03:47 AM

0 Likes
6
1784
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
‎2014-01-03 03:47 AM

What is the best way to connect a temperature sensor to an EGX300?

Hi there,

One of my customers asked me how to collect a temperature sensor to an already installed EGX300?

Do you have any recommendation?

Thanks in anticipation!

-Maxence

Tags (4)
  • Tags:
  • egx300
  • sensor
  • sim10
  • temperature
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 6
Randi_Dolan
Commander Randi_Dolan Commander
Commander

Posted: ‎2014-01-08 08:33 AM

2 Likes
0
1630
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
‎2014-01-08 08:33 AM

Hello Maxence,

If the temperature sensor is capable of communicating via Modbus, you can connect the sensor on the EGX300's RS-485 serial port.  You can then create a custom device type using the Custom Device Type Generator to view and log data from this device.

Randi

Reply
LaurentCoene
Captain LaurentCoene Captain
Captain

Posted: ‎2014-01-14 01:04 AM

0 Likes
1
1630
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
‎2014-01-14 01:04 AM

Hi Maxou!

Many ways to do that and it really depends on the temperature sensor. If it is Modbus like the CWLP from Veris, use the custom device type generator and you're done. Only problem with that is that Modbus temperature sensors are typically a little more expensive.

If you have a 0-10V. or a 4-20mA, you will need some sort of Modbus converter in between. For example, you can use the AI (Analog Input) of the SIM10M as described here. However it can get messy/tricky.

Frankly speaking, taking cost into consideration, I would replace the EGX300 by a Com'X200 which has two Analog Inputs. You can wire your 0-10 or 4-20 directly in, and you're done!

If you have many many sensors, then you should look at using some stuff from the building BU (maybe using the GW and EnOcean sensors....)...

Anyway, hope this helps!

Reply
dborle
dborle Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2014-01-14 04:25 AM

0 Likes
0
1630
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
‎2014-01-14 04:25 AM

Hi Laurent,

I agree with you. But it also depends, whether Maxence needs the capability of the EGX300 to show realtime data and logged data over the integrated web server or not (as the Com'X doesn't has this capability).

Cheers

Daniel

Reply
josgrafe
Lieutenant JG josgrafe
Lieutenant JG

Posted: ‎2014-02-01 02:43 AM

0 Likes
0
1630
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
‎2014-02-01 02:43 AM

We have connected an 0-10V sensor via a SIM10 module.

Reply
sesa205726_brid
Lieutenant JG sesa205726_brid Lieutenant JG
Lieutenant JG

Posted: ‎2014-02-05 01:37 AM

0 Likes
0
1630
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
‎2014-02-05 01:37 AM

In Italy, we have connected a temperature sensor to SIM10M. There are two way for to connect the temperature sensor to analog input of SIM10M. The features of the analog input of SIM10M are:

0-10 V with resolution of 0.01.

The featuring of the analog input implies two possible connection between devices:

1. if you use a PT100 you need a Crouzet convert to convert the current signal of the sensor in the corresponding voltage signal;

2. if you use a sensor with output directly in voltage, you can connect this one to analog input of SIM10M.

By

Reply
conchimunoz
conchimunoz Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2014-02-05 04:23 AM

0 Likes
0
1630
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
‎2014-02-05 04:23 AM

Hi!

We did this configuration before and we choose an OTB. OTB is a I/O distributed device  which can communicate in ModBus protocol and you can add on it a card for analog inputs  (4-20ma, 0-10v, pt100, pt1000, etc..). Then, in the EGX300, you can configure a custom device to communicate with the OTB.

You can read more information about Modbus OTB in this link:

http://www2.schneider-electric.com/documents/electrical-distribution/en/shared/interactive-catalogue...

I hope it helps.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.