SIM10M vs TWIDO for WAGES

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • SIM10M vs TWIDO for WAGES
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Kirk Romain_Polette Kirk
117
Guillaume_Evrard
Captain Guillaume_Evrard Captain
58
Randi_Dolan
Commander Randi_Dolan Commander
46
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Gateways and Energy Servers
Start a Topic
Anonymous user
Not applicable

Posted: ‎2014-06-02 10:36 PM

2 Likes
5
1319
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
‎2014-06-02 10:36 PM

SIM10M vs TWIDO for WAGES

Hi

I am designing a system that will have a large number of water meters as well as kWh meters and gas meters throughput a 30-odd levels commercial building.

I have elected to use the SIM10M pulse counter modules connected to several EGX100 gateways and into the PME.

Is there are any benefits of using TWIDO PLCs versus the SIM10M counter modules for this application?

FYI, there will be approximately 300 WAGES assets, connected to 73 pulse counter modules.

In addition, there will be about 250 electrical meters as well, but their design is sorted out.


Any comments would be appreciated.


Regards

Goran

Tags (3)
  • Tags:
  • sim10m
  • twido
  • vs
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 5
sesa149175
Crewman sesa149175 Crewman
Crewman

Posted: ‎2014-06-02 10:45 PM

0 Likes
0
1196
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
‎2014-06-02 10:45 PM

Hi,

you need to be careful while connecting the Pulse meters to SIM10M .for SIM10M Pulse frequency(Max 50Hz),duration of the pulse meter are important .

Regards

Ravi

Reply
LaurentCoene
Captain LaurentCoene Captain
Captain

Posted: ‎2014-06-02 11:50 PM

0 Likes
3
1196
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
‎2014-06-02 11:50 PM

I've seen both being used. In North-America, they tend to use the Twido, while in Europe/Asia I've seen more SIM10M being used.

Other than the cost, I'm not aware of any limitation but clearly, Ravi had a great insight!

Having said that, for so many I/Os, you could also consider the Automation Server from the Building BU with the UI-16 module which has 16 Universal Inputs. And you can put multiple of them together without additional power supply. It gives you the DI to Modbus needed as well.

That will give you some automation level that you could reuse or the connection to the UN2 or GW (Can2Go) in order to get some extra EnOcean of Zigbee sensors.

Really curious to see what others have to say! 🙂

Reply
LaurentCoene
Captain LaurentCoene Captain
Captain

Posted: ‎2014-06-03 12:28 AM

1 Like
0
1196
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
‎2014-06-03 12:28 AM

Hooo, nearly forgot. I've also seen the SmartLink used to collect pulses! You get 11 devices (for the one connected over modbus) or 7 if you use the Modbus TCP version. If you can get the pre-made wire (SmartLink --> Pulse), then it's a breeze! 

Reply
LaurentCoene
Captain LaurentCoene Captain
Captain

Posted: ‎2014-06-12 10:43 PM

0 Likes
1
1196
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
‎2014-06-12 10:43 PM

Related article about pulse that could interest other people: https://powersolutionscommunity.schneider-electric.com/docs/DOC-2550

Reply
Anonymous user
Not applicable

Posted: ‎2014-06-15 02:30 PM

0 Likes
0
1196
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
‎2014-06-15 02:30 PM

Thanks for your and Ravi's comments.

I have re-designed the system and decision is made to go with combination of both SIM10 and TWIDO. Simply, on floors where I had more than 6 utility meters (maximum per floor is 12 meters) i used TWIDO base module, and on floor where I had up to 6 utility meters I used the SIM10 module.

This way i saved on hardware, as i used one TWIDO instead of two SIM10 modules.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.