Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2013-12-0304:33 AM
SIM10M analogue value in EGX300 ?
We have connected an outside temperature sensor to the analogue input of the SIM10M which is connected to our EGX300.
When we read individual registers we can see a analogue value (register 25) . But the value is not displayed anywhere. And we can not select logging for the analogue value.
The digital signals are working fine. We are currently running on firmware 4.2 . Is updating to 4.350 helpful?
Link copied. Please paste this link to share this article on your social media post.
2013-12-1509:47 PM
Hello Jos!
I had written two articles about that. Can't remember the exact details, but they should help you as I always try to put as much details as possible for future references:
Also note that if you are going to push the data to Energy Operation, you don't have to worry about article number 2, and you're note limited anymore in terms of sensors since you can do all the math in the EMIS itself. (Just push the 4.20mA or 0-10V).