Firmware EGX300 v4.370

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • Firmware EGX300 v4.370
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Kirk Romain_Polette Kirk
117
Guillaume_Evrard
Captain Guillaume_Evrard Captain
58
Randi_Dolan
Commander Randi_Dolan Commander
46
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Gateways and Energy Servers
Start a Topic
JamesJeanette
Commander JamesJeanette Commander
Commander

Posted: ‎2014-06-30 09:57 AM

2 Likes
9
2504
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
‎2014-06-30 09:57 AM

Firmware EGX300 v4.370

RELEASE NOTES:

Updates:

Version 4.370 firmware provides:

  • Added Time-out for SMTP and HTTP Data Log Export
  • Updated ModbusTCP Client to handle connections closed by ModbusTCP Servers
  • Modified Data Log Export algorithm
  • Added Acti9 Dashboard functionality

   

Device Support:

  • Added the following devices
    • Vigilohm IM400
    • iEM3350
    • iEM3355
  • Added Input Metering Pulse Count to iEM3x55 and PM3255 Logging
  • Added Trending Support for the Conext TL
  • Updated ION7650 Reset Handling
  • Changed Micrologic E Min/Max Reset to reset both Min and Max values
  • Changed PM5350 "Total Energy" from "Energy Delivered + Received" to "Energy Delivered-Received"
  • Fixed issue with logging strings not matching topic for PM5100/PM5300, EM4800, PM5350xB, PM5350, and PM5500
  • Fixed issue with iEM3155 and iEM3255 not displaying Input 1 Pulse Weight correctly
  • Added check to PM3250 device type to determine whether or not to display Input Metering Values
  • Fixed Per Phase Power Trending in the iEM3150

Additional Product/Support Improvements




Attachments
v4.370.zip
Tags (13)
  • Tags:
  • 4.3
  • 4.370
  • acti9
  • conext_tl
  • dashboards
  • egx300
  • firmware
  • iem3350
  • iem3355
  • im400
  • smartlink
  • trending
  • vigilohm
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 9
sesa205726_brid
Lieutenant JG sesa205726_brid Lieutenant JG
Lieutenant JG

Posted: ‎2014-07-09 07:00 AM

0 Likes
0
2346
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
‎2014-07-09 07:00 AM

Hi , in the list of features of last firmware version of the EGX300 is not clear if EGX300 supports reading the PM5300 through TCP/IP connection.

Thanks

BR

Reply
avintola
avintola Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2014-10-13 11:22 PM

0 Likes
0
2346
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
‎2014-10-13 11:22 PM

James Jeanette

Hi, James! I have a quick question about firmware updates. When updating the firmware of EGX300, how will it affect the logged data in the unit and the current configuration. Will the logged data be erased and the configuration reverted to the default setup?

All the best,

Alyssa

Reply
JamesJeanette
Commander JamesJeanette Commander
Commander

Posted: ‎2014-10-14 10:09 AM

1 Like
0
2346
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
‎2014-10-14 10:09 AM

Hello Alyssa.

The logged data and configuration will remain; however, we do have some recommendations depending on which version you are updating from.

If you currently are running Firmware Version 3.7, follow this for 4.370:

4928

If you currently are running Firmware Version 3.8 (or GREATER), follow this for 4.370:

4929

*As a reminder.  You need both the Firmware file, and the Disk Update file to perform an EGX300 upgrade.  You apply the Disk Update file in the same manner (FTP) as the Firmware file, but only AFTER the Firmware file is transferred, and the EGX300 reboots.

I hope this helps.

James

FYI:

Reply
avintola
avintola Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2014-10-14 06:28 PM

0 Likes
0
2346
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
‎2014-10-14 06:28 PM

Thanks, James!

Reply
Jun_Escano
Lieutenant JG Jun_Escano Lieutenant JG
Lieutenant JG

Posted: ‎2014-10-21 01:36 AM

0 Likes
0
2346
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
‎2014-10-21 01:36 AM

Same here testing with the PM5320 but somehow it is not working (Via ION Setup i can get connection)

Reply
Jun_Escano
Lieutenant JG Jun_Escano Lieutenant JG
Lieutenant JG

Posted: ‎2014-10-21 01:41 AM

0 Likes
0
2346
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
‎2014-10-21 01:41 AM

Never mind i just forgot that the new firmware will fix this November 2014

Reply
JamesJeanette
Commander JamesJeanette Commander
Commander

Posted: ‎2014-10-21 07:02 AM

0 Likes
0
2346
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
‎2014-10-21 07:02 AM

This is correct.  The new version of EGX300 firmware will allow for remote ID connection to 255.

James

Reply
maxencevanhove
maxencevanhove Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2014-10-28 06:51 AM

0 Likes
0
2346
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
‎2014-10-28 06:51 AM

James, Hi!

Regarding the fix "Issue with logging strings not matching topic for PM5100/PM5300, EM4800, PM5350xB, PM5350, and PM5500", I'd like to understand if Active Energy was recorded under a wrong topic?


We currently have the following topics available under a PM5100:

5042

Would updating the firmware add Active Energy kWh to that list?

Thanks in anticipation!

-Maxence

Reply
arjanbijker
arjanbijker Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2014-10-30 09:56 PM

0 Likes
0
2346
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
‎2014-10-30 09:56 PM

HI James,

it seems that like logging of pulse count on the PM3255 is not working correctly.

Please see attached screenshots

50895090
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.