Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2013-02-2112:58 PM
EGX100 Firmware
Download the v.3000.zip file above to access the latest EGX100 firmware.
EGX100 Version 3.000 Firmware
This firmware version provides improved validation of the IP Address, and the IP Address / Subnet Mask combination.
To properly update the EGX100:
1. Transfer the version 3.000 firmware file (eg03000.bin) to your computer.
2. Via FTP, copy the eg03000.bin file from your computer to the root directory of the EGX100.
Do not remove power until programming is complete. Once the file transfer is complete, the EGX100 will automatically reboot. Refer to the EGX100 user’s guide if you need more information.
3. Verify that the download was a success by browsing the Firmware Version in the ‘Gateway Information’ section of the Diagnostics page.
Note: During firmware updates, communication to serial devices through the EGX100 is not available.