Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84773members
354212posts

ComX 200 Firmware Version 1.1 - new features, tangible benefits

Gateways and Energy Servers

Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.

JamesJeanette
Commander Commander
Commander

ComX 200 Firmware Version 1.1 - new features, tangible benefits

Firmware release 1.1 for the Com’X 200 Energy Server adds three key features that provide tangible benefits for customers.

  • Gateway functionality improves productivity since you can use the Remote Setting Utility (RSU) on your laptop to configure downstream devices without having to access them directly. This is done using the Modbus protocol.
  • Custom models library saves time and increases productivity. It enables the use of custom device types, such as devices with a shorter list of values to save time when defining the configuration.
  • Backup configuration settings to USB dongle is a feature that clearly helps save time during commissioning.

For more information on these features, check out the updated Com’X 200 user guide.

Download the Com'X 200 1.1 Firmware

James