Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84632members
353965posts

Heat Dissipation for LV component

Expert on Demand for Standards & Regulations

Solved
Widiyatmoko
Ensign
Ensign

Heat Dissipation for LV component

Does Schneider have heat dissipation table for all LV components like MCB, RCCB, RCBO, MCCB, ACB, CONTACTOR, ETC ?

@HelvinHermanT 

 

Tags (1)

Accepted Solutions
HelvinHermanT
Captain Captain
Captain
0 Likes
1
145

Re: Heat Dissipation for LV component

Selamat Siang Pak,

 

Untuk The Power/Heat Loss of iC60N MCBs & Vigi iC60 RCDs, bisa dilihat dibawah ini.

 

https://www.se.com/eg/en/faqs/FA233317/

 

Multi 9 Heat Dissipation.pngActi9 Heat Dissipation.png

See Answer In Context

Tags (1)
2 Replies 2
HelvinHermanT
Captain Captain
Captain
0 Likes
1
146

Re: Heat Dissipation for LV component

Selamat Siang Pak,

 

Untuk The Power/Heat Loss of iC60N MCBs & Vigi iC60 RCDs, bisa dilihat dibawah ini.

 

https://www.se.com/eg/en/faqs/FA233317/

 

Multi 9 Heat Dissipation.pngActi9 Heat Dissipation.png

Tags (1)
HelvinHermanT
Captain Captain
Captain
0 Likes
0
144

Re: Heat Dissipation for LV component

Silahkan cek link di bawah ini. 

How can I calculate the dissipated power (heat loss) inside a Blokset panel?

The amount of heat loss depends on the constituents of the panel (horizontal busbars, vertical busbars, circuit breakers, capacitors for power factor correction...etc). According to the heat dissipated from the panel. The attached calculator is a spread sheet used to calculate the heat loss in Blokset.

 

https://www.se.com/eg/en/faqs/FA279667/ 

Tags (1)