This forum is for engineers working EcoStruxure Building Operation, wanting to leverage the SEAL application to improve the efficiency in the engineering process.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2024-11-2104:31 PM. Last Modified: 2024-12-1005:13 PM
Welcome to the SEAL Community
SEAL is a toolbox with a number of powerful utilities to help automate and ease tasks that are usually cumbersome and time consuming. It comes with an easy to use DWG to TGML converter, and a versatile Script utility, which gives the user full access to automate EBO engineering, after deploying custom or standard applications of your choice. For some countries it is also used to create applications for EBO, but while the Design part is only applicable for those countries, the rest of the SEAL application provides value and efficiency to the engineering process regardless of the standards and process being used.
It comes with scripts for EBO to BACnet object conversion, generating trend logs based on naming patterns, advanced bindings (many to many) or search and replace functionality, fully automated duplication of devices or folders to specified paths and a few other cases. In addition to that, expert users can obtain the possibility to create own custom scripts, which they can share with the Community.